USART
Hi,Can i use usart instead of uart???RegardsAdrush
Ask questions, find answers, and share insights on STM32 products and their technical features.
Hi,Can i use usart instead of uart???RegardsAdrush
I'm new to micro controllers (but I have a software engineering background) and I decided to purchase a NUCLEO-F429ZI (STM32F429ZI).There are a LOT of pins on this board (168 I/O pins according to the datasheet!). However, if I just want simple HIGH/...
I am using CAN(MCP2515 Controller), I need to know the methods used to Test CAN Failure and Build in CAN Test.Methods I tried. 1: Checking Error Flag like Bus-Off Error Flag bit and Passive Error Bit, but due to Arbitration Failure Transmit Error Cou...
I have an custom STM32H743 TQFP100 board. I use I2C 4, PB8, PB9 at 100kHz.The code is generated with CubeIDE.The I2C_FLAG_AF flag on I2C4 is always wrongly set and the transmission after adress is aborted.The device sends an acknowledge.Is this an bu...
We are trying to use SPI1 as a slave to receive 11 bytes of data per transaction. I.E. SPI1_RX --> my_data_array[11] When an 11-byte transaction is received, we want the DMA to raise a flag that we will check (we can't afford to use interrupts, a...
The TIM12 update interrupt is not occurred in TIM8_UP_TIM13_IRQHandler().However it is occurred in TIM8_TRG_COM_TIM14_IRQHandler()I configured TIM12 update interrupt as below;//TIM4: master -> TIM12: slavevoid MX_Test_TIM4_TIM12(void) { NVIC_Enable...
I am using STM32F439NIHx MCU. After flashing the code, I removed ST-Link V2 from my PCand restart the MCU but our application is not working. But if I connect ST-Link V2 to my pc then my application is working. What is this problem? Please suggest a...
I have a feeling i know the answer to this is "just give it up" but I figure before I do that, has anyone managed to get this Atollic thing working with semihosting and the J-Link? I ran up against Atollic's libnosys.lib defining _lseek and some othe...
I am using the H7 and have a 10MHz sigma-delta ADC sending the Manchester signal. I do not have a clock going to the ADC because it generates its own.The internal DFSDM clock is set correctly, I think. I have a system clock of 96MHz and CKOUTDIV is s...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.