STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC Advice

Suppose you want to get the max sample rate out of the ADC and you can not use DMA, how would you do that?

ATo by Associate II
  • 2994 Views
  • 6 replies
  • 0 kudos

'F3 - RM316 COMP registers documentation

Please consider these modifications to RM0316:Also, please unify COMPxINSEL/COMPxINMSEL in that chapter (best by removing all instances of COMPxINSEL altogether - note, that in the registers table, the COMPxINPSEL bits are incorrectly marked as COMPx...

0690X00000DBylzQAD.png 0690X00000DByfhQAD.png

CAN2 peripheral configuration

I have this code attached which is configured to run both CAN1 and CAN2 peripherals however the TX functionality which is what I was trying to use is working on CAN1 but not on CAN2 (trying to send a packet using ADDmessage TX routine), I double chec...

NSood.1 by Associate
  • 767 Views
  • 0 replies
  • 0 kudos

STM32F723E-DISCO WM8994 audio codec

Hello,I try to use STM32F723E-DISCO to create guitar sound effect processor.At the begin I try to configure WM8994 codec to work in a simple loopback application LineIN to LineOUT (with small buffer in STM32 RAM memory). But without any positive resu...

H750 value line

I'm starting a project with stm32h750vb. Is it really worth it? I see that people are having problems with ADC, SDMMC, I2C. Are these problems inevitable with the H7 family?Btw, I want to make a 2 layer pcb with the h750, any advices?

BSant.1 by Associate II
  • 4854 Views
  • 11 replies
  • 0 kudos