For example, if two pins are set, via the Alternative Function registers, to be the rx and tx for a UART, but that UART is disabled, what state are the pins left in if the various GPIO registers are not changed?Does the rx pin remain an input, and th...