2019-09-03 6:05 AM
Hello, I have issues with STM32H743 UART. I use Nucleo 144 and I need to get GPS frames on UART7 (at 9600 baud) and display them on UART4 (at 115200 baud). If nothing is sent on UART4, reception of frames on UART7 is good but I want to display some values at the same time on UART4. If I do that, the frames on UART7 are not entirely received, some caracters are missing. More I print values on UART4 more there are missing caracters on UART7. Is that normal ? What can I do about this ? Thanks for your help !
2019-09-03 7:20 AM
WIthout seeing your code all we can do is make wild-#%$ guesses. My guess would be that you are using HAL and the polled version of HAL_UART_Transmit() and HAL_UART_Receive(). If that isn't it, post your code so we can give you better answers.
2019-09-03 8:05 AM
void log_print(const char *format, ...)
{
uint8_t fmt_idx = 0;
char pct = '%';
va_list args;
va_start(args, format);
while(format[fmt_idx] != '\0')
{
if(format[fmt_idx] == '%')
{
fmt_idx++;
if(format[fmt_idx] == 'c')
{
char arg = (char) va_arg(args, int);
HAL_UART_Transmit(&huart4, (uint8_t*) &arg, 1, 1000);
}
else if(format[fmt_idx] == 'd')
{
char message[11];
memset(message, 0, 11);
int arg = (int) va_arg(args, int);
sprintf(message, "%d", arg);
HAL_UART_Transmit(&huart4,(uint8_t*) message, strlen(message), 1000);
}
else if(format[fmt_idx] == 's')
{
char message[256];
memset(message, 0, 256);
char* arg = (char*) va_arg(args, char*);
sprintf(message, "%s", arg);
HAL_UART_Transmit(&huart4,(uint8_t*) message, strlen(message), 1000);
}
else
HAL_UART_Transmit(&huart4, (uint8_t*)&pct, 1, 1000);
}
else
HAL_UART_Transmit(&huart4, (uint8_t*) &format[fmt_idx], 1, 1000);
fmt_idx++;
}
va_end(args);
}void MX_UART4_Init(void)
{
huart4.Instance = UART4;
huart4.Init.BaudRate = 115200;
huart4.Init.WordLength = UART_WORDLENGTH_8B;
huart4.Init.StopBits = UART_STOPBITS_1;
huart4.Init.Parity = UART_PARITY_NONE;
huart4.Init.Mode = UART_MODE_TX_RX;
huart4.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart4.Init.OverSampling = UART_OVERSAMPLING_16;
huart4.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart4.Init.Prescaler = UART_PRESCALER_DIV1;
huart4.Init.FIFOMode = UART_FIFOMODE_ENABLE;
huart4.Init.TXFIFOThreshold = UART_TXFIFO_THRESHOLD_1_8;
huart4.Init.RXFIFOThreshold = UART_RXFIFO_THRESHOLD_1_8;
huart4.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart4) != HAL_OK)
{
Error_Handler();
}
}void MX_UART7_Init(void)
{
huart7.Instance = UART7;
huart7.Init.BaudRate = 9600;
huart7.Init.WordLength = UART_WORDLENGTH_8B;
huart7.Init.StopBits = UART_STOPBITS_1;
huart7.Init.Parity = UART_PARITY_NONE;
huart7.Init.Mode = UART_MODE_TX_RX;
huart7.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart7.Init.OverSampling = UART_OVERSAMPLING_16;
huart7.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart7.Init.Prescaler = UART_PRESCALER_DIV1;
huart7.Init.FIFOMode = UART_FIFOMODE_ENABLE;
huart7.Init.TXFIFOThreshold = UART_TXFIFO_THRESHOLD_1_8;
huart7.Init.RXFIFOThreshold = UART_RXFIFO_THRESHOLD_1_8;
huart7.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart7) != HAL_OK)
{
LOG_E("ERROR : UART 7 initialization");
Error_Handler();
}
}void GPS_getFrame(char* GPS_frame)
{
char uart_char = '\0';
uint8_t current_index = 0;
HAL_StatusTypeDef ret;
// read each character on the UART until '$' which is the beginning of a new frame
do
{
ret = HAL_UART_Receive(&huart7, (uint8_t*)&uart_char, 1*sizeof(char),1000);
if(ret == HAL_TIMEOUT)
{
LOG_W("HAL_UART_Receive return a timeout");
}
else if(ret == HAL_BUSY)
{
LOG_W("HAL_UART_Receive is busy");
}
else if(ret == HAL_ERROR)
{
LOG_E("ERROR : HAL_UART_Receive return an error");
Error_Handler();
}
__HAL_UART_CLEAR_FLAG(&huart7, UART_CLEAR_NEF | UART_CLEAR_OREF | UART_FLAG_RXNE | UART_FLAG_ORE);
} while(uart_char != '$');
// read and store each character on the UART until '\n' which is the end of the frame
do
{
if(current_index > MAX_FRAME_SIZE-1)
{
LOG_E("ERROR : Too much characters in the frame (maximum size : %d)\r\n", MAX_FRAME_SIZE);
Error_Handler();
}
ret = HAL_UART_Receive(&huart7, (uint8_t*)&uart_char, 1*sizeof(char), 100000000);
if(ret == HAL_TIMEOUT)
{
LOG_W("HAL_UART_Receive return a timeout");
}
else if(ret == HAL_BUSY)
{
LOG_W("HAL_UART_Receive is busy");
}
else if(ret == HAL_ERROR)
{
LOG_E("ERROR : HAL_UART_Receive return an error");
Error_Handler();
}
if(ret == HAL_OK)
{
GPS_frame[current_index] = uart_char;
current_index++;
}
__HAL_UART_CLEAR_FLAG(&huart7, UART_CLEAR_NEF | UART_CLEAR_OREF | UART_FLAG_RXNE | UART_FLAG_ORE);
} while(uart_char != '\n');
//log_print("%s", GPS_frame);
}Here is the init functions generated by MX Cube (for UART4 and UART7) and the functions I use to send data on the UART4 and to receive GPS frame on the UART7.
2019-09-03 8:13 AM
HAL_UART_Receive and HAL_UART_Transmit both BLOCK, you'll need to use a different scheme for concurrent comms
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.