cancel
Showing results for 
Search instead for 
Did you mean: 

what is the source of clock for CANBUS

VPras
Associate II

Hi,

what is the clock source for CANBUS in STM32F767?

I have referred the manual ,but still i cannot get the clear answer from it.

the main reason to know the clock source is to calculate the bit timing .

Thanks

Vimal

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

Usually the APB to which it is attached.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Hi,

my application is to create USB and CANBUS together.

1.when i use 16MHz crystal oscillator, i kept all PLL settings for max clock ,then USB is not working.

2. when i use 25MHz crystal oscillator ,CAN is not working.

what could be issue??

Thanks,

Vimal