STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

F4 or F3 board with ext. RAM and SD ?

Does anybody know a board with a STM32F4 of F3 with the following features:external RAM, 1 MByte or moreSD card interface, alternatively Debug port with VCP or ethernet interfaceA display would be optional.Had been looking at the usual suspects (ST, ...

Ozone by Principal III
  • 4943 Views
  • 13 replies
  • 0 kudos

Usage of HAL_SPI_Transmit

Hi,normally i use HAL_SPI_Transmit    HAL_GPIO_WritePin(Port, Pin, GPIO_PIN_RESET); HAL_SPI_Transmit(...)   HAL_GPIO_WritePin(Port, Pin, GPIO_PIN_SET);Is it possible to use it like following;   HAL_GPIO_WritePin(Port, Pin, GPIO_PIN_RESET); HAL_SP...

ACan.1 by Associate II
  • 1080 Views
  • 1 replies
  • 0 kudos

Stm32f4 adxl345 i2c not working? Std periph

I wrote code using the stm32f4 discovery card and adxl345 sensor using the i2c communication protocol. But Send data does not respond to my command. Please help me. I'll be crazy.#include "stm32f4xx.h" #include "stm32f4_discovery.h"     #define Max ...

HGök.1 by Associate II
  • 919 Views
  • 0 replies
  • 0 kudos

Transmitting multiple bytes through SPI

Hi everyone,I am trying to transmit multiple bytes via SPI.I could read the data through spi, so connections should be ok.Does anyone have idea what can be the reason, that I can not write data to the register of the slave?int writetospi(uint16 heade...

ACan.1 by Associate II
  • 2370 Views
  • 3 replies
  • 0 kudos

DAC+DMA stops while loop for 100 seconds

Hello everyone,I am very new in MCU programming and still learning it. I am doing a small project with DAC and Timers2,3 on STM32F429. DAC is trigger by time2 and timer3 is a counter which is triggered by a switch.Also, I have an LED blinking an a da...

MNajj.1 by Associate
  • 1603 Views
  • 2 replies
  • 0 kudos

How to stabilize and increase camera frame rate?

Hello, I've recently took over a project at my school where they are building a wearable camera. They have used STM32L496ZG as the MCU. Basically there are two sensors on the board: OV2640 and MLX90640. One takes regular JPEG and the other takes ther...

ESaat.1 by Associate
  • 1771 Views
  • 1 replies
  • 0 kudos

How to achieve 8nA in shutdown mode with wakup pin on L412?

Hello,I'm experimenting with ulp I'm starting from lowest power consumption achievable and add peripherals and wake up conditions to see what happens.That's why I'm starting with shutdown mode. I'm using a custom board with only an STM32L412K8, few c...

JulienD by Senior
  • 1949 Views
  • 6 replies
  • 0 kudos

Resolved! HAL_FLASH_Program not writing to flash permanently

Hi all,I am using HAL_FLASH_Program() to program an uuid into a specific address. I can verify it write successfully by reading from the address. However, if I power cycle the MCU, the memory at that address returns to the original value. If I write ...

vtran1 by Associate II
  • 9058 Views
  • 18 replies
  • 0 kudos