User Activity

STM32CubeIDE v.1.3.0STM32G431RBTxIn any timer if the input channels 1 and 2 are set for use as "Combined channels = Encoder Mode" (by CubeMX or integrated in CubeIDE), it is not possible to select a remapped input (for example from the comparator). T...
STM32CubeIDE 1.3.0I added the "USE_FULL_LL_DRIVER" symbol in my project properties:Subsequently I used "Device Configuration Tool" to re-generate the code (even without having made any configuration changes). At the end of the generation, the previou...
Some time ago I tried your STM-STUDIO: I found it very rough and can only be used for laboratory debugging.Why don't you plan to build a more flexible debugger that can then be used by the end customer to view internal data or change parameters?If yo...
With STM32G4 the use of counters to decode signals from quadrature encoders has been significantly improved. Furthermore we can use the comparators to detect the counting front and save external pins avoiding to make the signal come out from the comp...
See the attached project. If I go to change the settings of ADC1, in the "parameter settings" increase the number of conversions from 2 to 3. In the following lines "Rank 3" should appear, but it does not appear:If I try to switch to another peripher...
Kudos from