STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Unable to wake-up from stand-by using pin wake-up

Hello,I'm using STM32F779NI.I'm trying to enter Standby mode & would like to wake-up through pin wake-up (PC13).Looks like stand-by entry is happening fine (SBF is set post reset) but wake-up pin flag is not set.Please find the code as belowint main(...

STM32H743 DMA have some bug when I using lastest HAL lib

We check stm32h7xx_hal_spi.c, and Surprise that the lastest HAL Lib still not support HAL_SPI_DMAStop() and HAL_SPI_DMAResume(). It is very important. We found DMA_SxCR's EN bit out of control in some time.  We use DMA to send and receive spi dat...

YZhon.1 by Associate II
  • 1808 Views
  • 3 replies
  • 0 kudos

DMA Performance

Do some homework assigned by the lecture but have no direction so ask for some help.I need to write a function DMASpeed() to demosntrate the speed improvement of DMA over a software loop for memory to memory transfers. I include polling DMA for my ho...

Cl.1 by Associate II
  • 742 Views
  • 0 replies
  • 0 kudos

STM32L073 - Init RTC via external clock (PC)

Hi, ​My client has an existing circuit which is logging some data (no information given)Until the logging just has a counter which starts, when a power source is connected.Now they want to add a real clock to the logging entry, and I saw that the STM...

LSchm.1 by Associate II
  • 5843 Views
  • 9 replies
  • 0 kudos

Resolved! STM32F1 PC14 and PC15 don't be output ?

Posted on February 21, 2018 at 13:01Hi;I have a problem.I want to be output pins PC14 and PC 15, so make the registers PWR -> CR = 0x00000100, RCC-> BDCR = 0x00000000. probably  LSE ocillator isn't off. thim my code :#include 'stm32f10x.h'#include '...

I'm trying to use the MultibufferDMA mode of HAL driver for STM32F769 device. There's not a single example I could find which uses this mode in the list all the applications/demos/examples for STM32 devices. Here's an example call I use :

 // using Double-Buffer DMADMA_HandleTypeDef hdma ;StreamBaseAddr = DMA_CalcBaseAndBitshift(&hdma) ; // get the stream base addr if (HAL_DMAEx_MultiBufferStart_IT(&hdma, StreamBaseAddr, Buffer[0], Buffer[1], BUF_SIZE))     {       Error_Handler();   ...

canbu22 by Associate III
  • 2734 Views
  • 3 replies
  • 0 kudos