STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L476RG Compilation Issue: Missing Headers

Hi, I've been trying to compile a program to talk to a sensor over UART for my STM32L476RG board. I'm having an issue with that I've tidied up the library that is needed to talk to the sensor, but I'm getting errors that I'm missing header files such...

0693W000001pkOeQAI.jpg
NStep.1 by Associate
  • 2203 Views
  • 2 replies
  • 0 kudos

STM32L010 low power mode

   In an attempt to reduce power for a critical battery powered system, I tried, without success, to make the chip run in the power range 3 (1.2V). Here is what I do:   At power up, with the chip running from the MSI clock divided by 2 (1Mhz), whatev...

adaniel by Associate III
  • 800 Views
  • 0 replies
  • 0 kudos

Wake STM32L4xx from SHUTDOWN using RTC Alarm?

I'm currently using the STM32L4R9I-EVAL board and trying to prototype an application where the microcontroller will need to be in lowest power (i.e. SHUTDOWN) mode for several days or weeks and then wake up to perform an action. I can get the the mi...

Interpretation of SPI communication error

Hello,Still struggling with my SPI setup.See https://community.st.com/s/feed/0D53W000006r3jX for details on SPI and GPIO settings.On the exact same setup I have sometimes a correct communication and trace is :SCK in yellow, MISO in blue. I send bytes...

0693W000001pn8oQAA.png 0693W000001pn98QAA.png
Gpeti by Senior II
  • 1992 Views
  • 4 replies
  • 0 kudos

How to use flash loader demonstrator to program STM32F427VI

Hi all,I have the STM32F427VI connected using serial RS232 cable.I downlaoded the latest version of the Flash Loader and the parameters are Even/115200/Disabled/8I tried using jumper on boot 0, boot 1 and boot 0&1 but I can't connect to the MCU.Any i...

As.51 by Associate III
  • 1773 Views
  • 3 replies
  • 0 kudos

stereo I2S communication

I am using STM32F103C for mcu and SPH0645 model for microphone.When I connect only one microphone and communicate with I2S it works!then I wanted to do make stereoSo I connected two microphones one with SEL=0 and the other with SEL=1However, WS gives...

JAn.1610 by Associate II
  • 3214 Views
  • 7 replies
  • 0 kudos