cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H743 DFSDM, PDM Microphones

NHend.7
Associate II

Hi

I am using the Stm32H743 Nucleo Board.

I followed the app note to use the DFSDM(https://www.st.com/content/ccc/resource/technical/document/application_note/group0/7d/62/3d/ad/24/57/47/78/DM00380469/files/DM00380469.pdf/jcr:content/translations/en.DM00380469.pdf).

The Mics used is the IM69D130(https://www.infineon.com/dgdl/Infineon-IM69D130_Microphone_Shield2Go-GS-v01_00-EN.pdf?fileId=5546d462677d0f4601677f3486ed0941)

I have the STM32H743 running at 480MHZ.

DFSDM is 60MHz.

CLK DIV 25.

The FOSR 50

Over sampling is 1.

It is running on the dma on half call back and full call back.

the arrays are shifted to the left by 8bits

The two data arrays are interleaved.

The play buffer is always at max data.

Kind Regards

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
waclawek.jan
Super User

Is there any question?

JW