STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with STM32g070 ADC

Hi,I got a problem with STM32G070RBTx ADC configuration. I configured ADC in interrupt mode. After each conversion I change channel to measure different pin. I got 9 pins to measure(PA0 - PA7 and PB12). With PINS on PORTA I got no problem but PB12 is...

Olek1 by Associate II
  • 1770 Views
  • 3 replies
  • 0 kudos

STM Studio in snapshot mode for STM32CUBEIde

Hi,I am trying to use the STM Studio in snapshot mode but I got some errors.1) Core/Src/acqTrigger.c:310:16: error: '_FAR_DATA_' undeclared 2) Core/Src/dataAcq.c:228:17: error: 'g_dataTraceBuffer' undeclared And other...There is any explanation of ho...

DKuro.1 by Associate III
  • 1174 Views
  • 1 replies
  • 0 kudos

STM32G030J6 Reset in loop

Hi, I have a STM32G030J6 with a trimpot connected to PA0 (NRST), but I need to disable NRST function. Based on pdf (UM2568) I write this:<code>uint32_t nrstmode; /* Enable Flash access anyway */ __HAL_RCC_FLASH_CLK_ENABLE(); /* Unlock flash */ FLASH-...

MCost.1 by Associate
  • 1514 Views
  • 1 replies
  • 0 kudos

ADC external trigger input

Hi I'm developing an application which I tested on the nucleo board and I want to make my custom board. I went through the datasheet of STM32Go71kb(32 pin version) and I could not find the ADC external trigger input pin. Additonally I cannot provide ...

BDasa.1 by Associate II
  • 1590 Views
  • 0 replies
  • 0 kudos

Resolved! problem when changing from DTCM Ram to RAM_D1

Hello, I am writing a project with STM32H7. The project contains RTC, SPI, USART, SD Card, timers, and I2C. In order to have more RAM, I have brough the data and bss to RAM_D1. As next steps I want to implement Ethernet. However, I realized that in o...

VYoun by Associate III
  • 8713 Views
  • 12 replies
  • 0 kudos

STM32L011F3 ADC Calibration

Hi Sir,In STM32L0 ADC, there is a feature call ADC calibration.I would like to know, after performing ADC calibration, do I have to do factoring using the CALFACT (calibration factor obtained after running ADC calibration) in the result I obtained fr...