STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F767 QUADSPI with DMA

I've referred STM32F769I_EVAL QSPI with DMA source code and implemented same way for STM32F767 but its not working. can anyone provide the sample code for STM32f767 QSPI with DMA

AShel.1 by Associate III
  • 4658 Views
  • 6 replies
  • 0 kudos

RTC milliseconds on STM32F413CH

Hi,I would like to know if is it possibile to manage milliseconds using internal RTC.If it is, please can you specify the code to get milliseconds information.Thanks for your support

SGIUS.1 by Associate
  • 936 Views
  • 1 replies
  • 0 kudos

Brown Out Detection

I am using STM32F779NI for my project. My use case is I want to detect brown out reset after brownout occurs and system restarts.I am checking brownout reset flag using if (__HAL_RCC_GET_FLAG(RCC_FLAG_BORRST). But the problem is this flag is shared/c...

A3 by Associate III
  • 10258 Views
  • 5 replies
  • 0 kudos

hi i am using STM32f746zg microcontroller with CANBUS i want to establish communication between CAN1 and CAN2 where CAN1(master) will send and CAN2(slave) should receive. CAN1 is transmitting perfectly but it is not receiving at CAN2 ..

can anyone help me with the code ....thanks in advance here is my codestatic void MX_CAN1_Init(void){ /* USER CODE BEGIN CAN1_Init 0 */ /* USER CODE END CAN1_Init 0 */ /* USER CODE BEGIN CAN1_Init 1 */ /* USER CODE END CAN1_Init 1 */ hcan1.Instance =...

B Vinod by Associate II
  • 932 Views
  • 0 replies
  • 0 kudos

Resolved! What is the Actual Input Clock Source for TIM1 of STM32F103RG?

I found from ref manual that the internal clock source for TIM1 is APB2 pre-scaled value.(Please see attached image).From CubeMx, I've configured my main clock frequency to be 48MHz, which is a PLL multiplied value from external crystal oscillator of...

0693W000001sv68QAA.png 0693W000001sv6IQAQ.png 0693W000001sv8xQAA.png
SShid by Associate III
  • 4462 Views
  • 4 replies
  • 0 kudos

Resolved! Restart MCU via software

Hi, How can I restart stm32l431 via software? I an using the MCU with sim800l and I can be able to restart MCU using text message. Does Exist some HAL function to restart MCU?

GFont.1 by Associate III
  • 1753 Views
  • 3 replies
  • 0 kudos

where is eStore order status??

Hi,I just order some stm toolkit from eStore and my question is where is order status ?? https://www.st.com/content/st_com/en/sample_and_buy/sample-and-buy/buy-from-estore.html

CChun.2 by Associate
  • 1933 Views
  • 0 replies
  • 0 kudos

Open source Bluetooth Apps for Addressable RGB's

Hi all!Been a loooong time since I've been around forums, but I'm back!So a long time project I've wanted to do is coming back into my brain and I figure its time to start chipping away at it!I love RGB LEDs, especially the addressable variety, and I...

STM32F103C6 never enters interrupt handler and because of that holds SCL low because of RxNE is set, BTF is set and DR hasn't been read after first data byte received, stopping reception, why?.

I'm trying to send some data from master to a slave (the STM32F103C6) with HAL functions, with HAL_I2C_Slave_Receive() -no interrupt mode- the reception works flawlessly but with HAL_I2C_Slave_Receive_IT() -the one needed- the slave acknowledges its ...

VRami.1 by Associate III
  • 903 Views
  • 0 replies
  • 0 kudos