STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

[STM32F412] Changing system clock issue

I am trying to change the system clock on my STM32F412 discovery board to 100 MHz using the HSI, however it just seems to crash. I am using direct writes to registers, but I looked at pregenerated CubeMX code and my registers look the same for the cl...

MB.2 by Associate III
  • 2197 Views
  • 2 replies
  • 0 kudos

exti1 interrupt works not fine....

HiI am developing a product using stm32f429.​case 1>- use cmsis_rtos2- Interrupt is generated every 20ms using exti1(PA1).- In exti1 callback function, execute gpio is set > delay 1ms > reset.​case 2 >- case1 + fmc initialize codecase 1 works fine. H...

ssooki by Associate III
  • 5603 Views
  • 9 replies
  • 0 kudos
lm.1 by Associate II
  • 1847 Views
  • 5 replies
  • 0 kudos

STM32F407 UART problems. PuTTY, FTDI USB to TTL converter

EDIT: For crying out loud. Why is half of my code chopped off? #if !defined(__SOFT_FP__) && defined(__ARM_FP) #warning "FPU is not initialized, but the project is compiling for an FPU. Please initialize the FPU before use." #endif   #include "stm32...

AAnth.1 by Senior
  • 3018 Views
  • 6 replies
  • 0 kudos

STM32 I2C Issue

Dear friends,I am using STM32f407vgt6 and a DS3231 RTC module and I use I2C1 peripheral to read date from DS3231. It is working fine but after 10 or 12 minutes the I2C bus is continously BUSY and I do not know what to do.Is there any way to control t...

Mujtaba by Senior
  • 1796 Views
  • 2 replies
  • 0 kudos

Resolved! Starting Tim2/3/4/5 Slaves with HRTIM-SyncOut does not work

Hi,i am desperately trying to start multiple Timers with the HRTIM as single trigger.The datasheet states, that internal trigger connection "tim_itr10" is "hrtim_out_sync2".So I enable the HRTIM-Master-TimerHRTIM1->sMasterRegs.MPER = 0xFFDF; HRTIM1->...

Albi G. by Senior
  • 3811 Views
  • 6 replies
  • 0 kudos

Resolved! STM32H745XI dual core debugging and flashing

Hi all,I'm attempting to run the simplest example code provided for the STM32H745XI dual core (M7 and M4 cores). I've configured my cube debugger as explained in the link below, and I'm having no success debugging or even starting the second core (M4...

TypeKazt by Associate III
  • 6879 Views
  • 11 replies
  • 0 kudos

STM32H7 and SPI interface

I'm working with the STM32H7 MCU and I have three memories (1 flash, and 2 fram) connected to SDPI1 interface. According to flash datasheet, max SPI clock can be up to 80MHz. Nevertheless, when having the SPI SCK set at 7.5MHz (SPI peripheral clock i...