STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! HAL Timer PWM Instance and Init parameters error with ADC1

Hello,I am working on STM32F413VGT with STM32CubeIde.I am using timer 3 channels 1 and 2 to generate 2 PWM signals to control a motor. This part works perfectly.I am also using ADC1 in DMA mode to get 7 ADC measurements. This function also works perf...

0693W000001t6okQAA.png 0693W000001t6pnQAA.png
TGate.1 by Associate II
  • 9528 Views
  • 8 replies
  • 0 kudos

How Indication works

Issue: How to send indicationhow can get confirmationHow to disable indication from server to clientHow to know client all data received from serverMy Code is:       bool isIndicationEnable;       if (attribute_modified->Attr_Data[0] & COMSVC_Indicat...

Debug

Hello STM community, I'm using a STM32 L476RGB NUCLEO with a XNucleo 53l0a1 I want to make the process of calibration but I have a problem when I compile my main program i get this error showing anyone know what i should do? you can see the screenTha...

MSAMB.1 by Associate III
  • 1353 Views
  • 1 replies
  • 0 kudos

Resolved! Probleme on getting clock signal on SPI slave device,

Hi ,i have a problem with SPI slave device, it doesn't receive the clock signal from stm32f103 (Master), i have configured the baud rate correctly : 72Mhz/32 (SPI1), which is inside the range clock freq of slave device, CS pin is active low so when i...

0693W000003BDzzQAG.png 0693W000003BDzpQAG.png 0693W000003BDzfQAG.png
SIDRI.1 by Associate III
  • 1012 Views
  • 1 replies
  • 0 kudos

Communication with interrupt between 2 cores

Hello,I am trying to communicate with interrupt between the Cortex M4 and M7. I tested the HSEM but, maybe I'm wrong, the semaphore locks a process when it waits for it.Thanks for you help

OADDI.1 by Associate II
  • 1891 Views
  • 3 replies
  • 0 kudos