cancel
Showing results for 
Search instead for 
Did you mean: 

RM0440, Rev 2, STM32G4 Series reference manual - Timer controlled OpAmp input mux documentation suggestions

Singh.Harjit
Senior II

Section 24.3.8, page 752, third paragraph says:

"The inverting and non inverting inputs selection is performed using

the VPS_SEL and VMS_SEL bit fields in the OPAMP switch control register."

The "switch control register" should be "timer controlled mode register".

Sections 24.5.1 to 24.5.12 titles have "x" and (x = 1..6) in them that they shouldn't?

Examples:

24.5.1 OPAMP1 control/status register (OPAMPx_CSR) (x = 1...6)

should really be:

24.5.1 OPAMP1 control/status register (OPAMP1_CSR)

because there is a different one for OPAMP2:

24.5.2 OPAMP2 control/status register (OPAMPx_CSR) (x = 1...6)

this should be:

24.5.2 OPAMP2 control/status register (OPAMP2_CSR)

I haven't looked to see if the (x = 1..6) approach will work and all of them can be combined.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Imen GH
ST Employee

​Hello,

Thank you for the remark

I will check

Regards

Imen GH
ST Employee

Hello

We will correct typos in the coming release of the RM.

Best Regards,

Imen