STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to configure and program MPU (memory protection unit ) of STM32L4A6ZGT6U ? OR any example code of MPU for STM32L4A6ZGT6U

HI All, I am currently using STM32 nucleo-L4A6ZG development board.I want use MPU of STM32L4A6ZGT6U.But i am very new with STM32 nucleo-L4A6ZG development board.So is there any example code of MPU with STM32L4A6ZGT6U ?So i can start with that .Than...

RMane.1 by Associate II
  • 1714 Views
  • 2 replies
  • 0 kudos

SWD connection not working

Dear,I encounter an issue when working with STM32L4 SensorTile Board. I normally load projects from MDK-ARM to my project normally, but now when I load the project, it loads in the software normally, but the circuit does not seem to work as normal. I...

TNguy.10 by Associate II
  • 1203 Views
  • 1 replies
  • 1 kudos

Resolved! STM32H7 Nucleo Board (NUCLEO-H743ZI2)

Hi,we are having difficulties in order to find solution for STM32H7 Nucleo Board (NUCLEO-H743ZI2). When we are trying only toggle a pin ( interrupts are closed --> 480MHz)freq is not passing 20MHz. When i check ref documents GPIO section, it says “F...

MTARH.1 by Associate II
  • 2070 Views
  • 2 replies
  • 0 kudos

How can I send data from STM32H747 to computer ?

Hello,I successfully sent data from the STM32H747 to the computer using USART1 via usb. Nonetheless, I can't find any solution to send data from the computer to the STM32. Any ideas on what communication protocol and medium I could use ?Data are comp...

Resolved! Avaiability of STM32H72x / STM32H73x

Updating to CubeIDE 1.14.1 I have seen that I can choose some new STM32H7xx MCU's ( especialy the STM32H725, STM32H735 and STM32H730 ). They are very interresting for me ( 3. CAN interface and 2x OCTOSPI with hyperflash support ). Is there any roadma...

MHoll.2 by Senior III
  • 1604 Views
  • 3 replies
  • 2 kudos

Resolved! How to calibrate ADC value on STM32F413 series micro controllers ? There is so much noise without giving analog signal on analog pin ?

I am getting so much noise on analog pin without connecting any analog signal. I also tried by changing analog pin but still i am getting so much of noise in analog pin. I am calculating analog value for 50 Hz signal. Is there any way to calibrate S...

MGami.1 by Associate III
  • 2503 Views
  • 6 replies
  • 0 kudos

VCom port not working with 767 ZI board.

I have found a few tutorials about implementing a vcom port with STM32, and I could successfully programs (well, let's not exagerate let's say I merely generated programs) working for discovery F407 and F469. I could send a constant string that I rec...

PG.1 by Associate III
  • 587 Views
  • 0 replies
  • 0 kudos

Dear fellow geeks, We'r using a Nucleo-f103RB to program a STM32L010k4T6. We ar able to write a PIN high and write a pin LOW we can also use the SPI. The only problem we have is with uart. We can't seem te get it to work.

In the datasheet https://nl.mouser.com/datasheet/2/389/dm00440565-1799229.pdfis stated that the uart and the SPI are part of two different alternate functions. The error message and the code will also uploaded if needed.

0693W000003CCXcQAO.jpg
Rgoss.1 by Associate II
  • 998 Views
  • 1 replies
  • 0 kudos