STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

We are using this ic STM32F103VET6 and Oscillation of 8 MHz Crystal with through capacitor of 22pf i am not getting the Oscillation from the microcontroller ?

We have two same design Board, one is fabricated in last year, another one is this year fabricated boards and i loaded same code for both boards.Achivally this year what i fabricated with little changes on the Connector side and we are used buffer ic...

SMudi.1 by Associate
  • 1415 Views
  • 2 replies
  • 0 kudos

Changing data advertisement frequency on BlueNRG DK example

Hello, I am using the example code BLE_Throughput from the BlueNRG-2 DK to program a PCB. The example is working fine but the frequency of advertisements is too high for what I need and I could not find in the code where can I change it. Could someon...

CFred.1 by Associate
  • 875 Views
  • 0 replies
  • 0 kudos

CAN mystery. Receiving messages but not able to send

Hi.I have a program that sometimes fails to send data on CAN but still receives them correctly.This is on an STM32L462 using 1.4.2 IDE and latest API.For some unknown reasons, at one moment, out mailboxes never empty. It can be anytime from right upo...

STM32H745 Maximal performance configuration

I'm working in a project that involve a thermal camera image processing.I need to process a buffer of 384*288 (16bits) in fastest way possible.I'm using the 480Mhz VCO template to set the procesor in 400Mhz (Cache enabled).I already did some code op...

Jvela.11 by Associate II
  • 1941 Views
  • 2 replies
  • 0 kudos

STM32F413 - Delay at the end of UART transmit

Hello,I am encountering an issue with the STM32F413 MCU: when transmitting data over UART, there is a short delay between the stop bit of one byte and the start bit of the next byte when transmitting data one byte at a time. I compared the behavior o...

0693W000002la33QAA.bmp 0693W000002la6bQAA.bmp

Resolved! q15 fixed point 1.15 9.7 etc

HelloI was wondering about nubering in q15 fixed pointI am guessing that in 1.15, 1 (msb) is responsible for sign and 15 bits are for magnitude(I could be wrong)However what does 9.7 mean ? does it mean 9 bits are for whole numbers and 7 bits represe...

hashtala by Associate II
  • 1881 Views
  • 2 replies
  • 0 kudos

Mistake in STM32G4xx Reference Manual (RM0440)?

The STM32G4xx Reference Manual (RM0440) Rev 4, Figure 2, "Memory Map" on Page 81 says Option Bytes 1 is from 0x1fff7800 to 0x1fff7810 (16 option bytes), Option Bytes 2 is from 0x1ffff800 to 0x1ffff810 (16 option bytes).However:Table 7 on page 94 says...

Current Consumption of STM32G071GB in deep sleep mode?

What is the current consumption of STM32g071GB in deep sleep mode? I found the tables of current consumption in the datasheet, but I am not certain which is the deep sleep current among the list. I have seen the following:

0693W000002lbbQQAQ.jpg
Naig by Associate II
  • 2342 Views
  • 5 replies
  • 0 kudos