Posted on October 24, 2017 at 06:21When I meet a bad block in a NAND flash,it will stop here forever.The 'tickstart = HAL_GetTick()' should put in front of 'while(HAL_NAND_Read_Status(hnand) != NAND_READY)'.#nand-flash-driver #stm32cubemx #bug
I know that.Because the volatage for the core actual needed is 1.38V. The internal SMPS output voltage is too big. It will make IC more heater. As to,why internal LDO can run at 480Mhz, in my opinion, it is that the LDO area of the chip can...