STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I am using STM32F4 processor. The problem I am seeing is that at times the processor resets and the CSR register reports 04 in reset cause which is NRST pin reset. Problem is that we do not see any reset on the NRST Pin.

Scope is configured correctly. Reading of CSR register is done way early in the code and is reliable. Register is cleared after reading. Scope is configured correctly.When we trigger pin reset externally, we can catch it on the scope. When we trigge...

RBharol by Associate III
  • 3463 Views
  • 4 replies
  • 0 kudos

Examples of using the HAL libraries for using I2C as both master and slave on a single I2C interface, i.e. in a multi-master configuration?

Hi there,I'm trying to implement a multi-master I2C network, where there are several nodes (around 6), any of which can send a message to any other. In other words, all nodes usually acting as slaves, waiting for incoming I2C messages. When any node ...

JElso by Associate II
  • 4452 Views
  • 4 replies
  • 0 kudos

Resolved! Interfacing code of Ws2812b on stm32F1 is working but in a same way when i am trying it with Stm32F4 it is not working !!!!

TIM_HandleTypeDef htim3;DMA_HandleTypeDef hdma_tim3_ch2;/* TIM3 init function */void MX_TIM3_Init(void){ TIM_ClockConfigTypeDef sClockSourceConfig = {0}; TIM_MasterConfigTypeDef sMasterConfig = {0}; TIM_OC_InitTypeDef sConfigOC = {0}; htim3.Instance ...

Resolved! I have a question about the STM32H743...

If this device is powered-down (i..e voltage is 0 on all rails), what impedance will be presented by the Port pins? If a pin from a powered-down STM32H743 is connected to a pin on another (fully powered) device, what current drain will occur?

Question about STM32H743 Errata Sheet ES0392 Rev 7

In Section 2.2.13 of ES0392, it states that there is "unexpected leakage current" if Vin >Vdd.What is the bound on the leakage current (assume an FT pin type):Vin = 5V and Vdd = 1.8VVin = 5V and Vdd = 3.3VVin = 3.3V and Vdd = 1.8VThank you.

losing some isr

Hello dear experts,I am using the TIMER2 on stm32F446Re with TI1_ED as reset mode input and TIM2_CH4 as timer value capture input. I inserted code to toggle a gpio in the HAL_TIM_IC_callback. On the scope I am capturating the TIM2_IC4 signal and the ...

papageno by Associate III
  • 1376 Views
  • 2 replies
  • 0 kudos

ADC DMA with TIM21 TRGO conversion source on STM32L010

I've got an application where I'm performing an ADC DMA transfer where the ADC conversions are triggered by the TIM2 TRGO. Everything was running smoothly until a PCB respin forced me to switch over to TIM21 to trigger the conversion. I didn't see a ...

DWann by Associate III
  • 5622 Views
  • 12 replies
  • 0 kudos