STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F405 IWDG doesn't reset

I am having a problem where the IWDG seems to not reset the processor. I have setup a very simple project that enables the IWDG and then doesn't pet it - it should reset, but it doesn't. Running under the debugger or running standalone, it doesn't re...

GPIO toggle example not toggling in BLUENRG 232 MCU. THe program is running and the DAT resistors changing values.

/******************** (C) COPYRIGHT 2015 STMicroelectronics ********************* File Name     : GPIO/IOToggle/main.c * Author       : RF Application Team* Version      : V1.1.0* Date        : September-2015* Description    : Code demostrating the G...

UART DMA Capture Restart.

Hi, I need a little help with this situation.I have to receive a packet from a serial port, this packet has a variable size and is also quite long. So I use two areas of RAM as a buffer and alternatively send the data to an external flash. I tried us...

Resolved! How to close the IWDG when STM32L051 enter stop mode.

when I use STM32L051, its iwdg and stop function ,after it enter stop mode ,the iwdg is also working,I want to close the iwdg when it's stopped,but I didn't find this bit of "IWDG_STOP" in FLASH_OPTR register ,so I don't know how to do ,because I use...

0693W000005AIl0QAG.png
泽陶.1 by Associate II
  • 3025 Views
  • 4 replies
  • 1 kudos

Adapting Custom Keyboard GUI to multi-screen application

I have been fighting to get the keyboard adapted to a multi-screen application for several days. I have gone thru the code generated by the Custom Keyboard GUI and the code that I have adapted for my application. I just don't see how to get the keybo...

LDoyl by Associate III
  • 690 Views
  • 0 replies
  • 0 kudos

Problem with simple I2C read on STM32F105

I am simply trying to read a few bytes from an I2C memory device using the following code: uint8_t buff[ 4 ]; HAL_I2C_Mem_Read( &hi2c1, ( uint16_t )( 80 << 1 ), 0, I2C_MEMADD_SIZE_16BIT, buff, 4, 10 );However, when I look at the output on the ...

0693W000005ANzHQAW.png

Resolved! STM32F103RGT6 - Confusion about adc pins

Hello.I want to use ADC in my STM32F103RGT6 Uc, but I don't understand what pdf's says about where the pins are.In this document We can see, that there are 3 ADC converters: ADC1, ADC2, ADC3.However, reading further on page 29, I can see alternate fu...

fifi_22 by Associate III
  • 1296 Views
  • 1 replies
  • 0 kudos

Apparently a conflict when clearing TC flags of DMA2 Streams

Hello to all, I hope you and your families are safe and sound. I am working to improve my project based on the STM32F469 MCU, but now I am experiencing a weird behavior. I can't post the code of course, too many files connected, so I will try to expl...

Digimorf by Associate III
  • 5183 Views
  • 8 replies
  • 0 kudos