STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 as I2C slave - sporadic errors - how to diagnose?

EDIT: Note change of direction of things in 3rd post.I have a stm32f091, which has a program that basically runs one mainloop that triggers ADC measurements and polling values from i2c chips using the i2c2 peripheral in master mode. ADC uses a DMA ir...

SKled.1 by Senior II
  • 1963 Views
  • 2 replies
  • 0 kudos

STM32F072RB Jitter/Delay

Small delays occur in projects and tests. The delays are usually about 6us. They also occur with simple calculations. What can be the reason? I have already tested with a new project without functionalities.

MF.2 by Associate
  • 3234 Views
  • 3 replies
  • 0 kudos

H743 FDCAN - Data Time Segments ignored?

Hello,I am trying to setup CAN FD between 2 Nucleo H743ZI2 to transmit data at a relatively high speed (shooting for 4 Mbps), however, I am experiencing issues getting the data part of the frame to use its own timings.I set FD CAN and normal mode, tr...

Smoun.1 by Associate III
  • 6977 Views
  • 4 replies
  • 1 kudos

SDRAM interfacing issue

I am using 12.1" TFT Display of 800x600 resolution and interfacing it with STM32F429BI Micro-controller and IS42S16400J SDRAM .I am getting the flickering issue in my display. When i by pass the SDRAM it working ok , there is no flickering, but on co...

DPRAJ.1 by Associate II
  • 3473 Views
  • 3 replies
  • 0 kudos