STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! HAL_TIM_PeriodElapsedCallback() refuses to trigger

GreetingsI have attempted to write an application, to toggle the LD4 LED (On PD12) on the STM32F407VGTx Discovery board. I am toggling the LED, on interrupt, when the timer overflows. I have placed the HAL_GPIO_Toggle() in the HAL_TIM_PeriodElapsedCa...

LSlat.1 by Associate II
  • 8285 Views
  • 6 replies
  • 2 kudos

interrupt on receiving bytes via SPI HAL

help me please. working in stm32cubeide. I can not enable interrupt on receiving bytes via SPI via HALmain.c/* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h"   /* Private var...

k.s.corp by Associate II
  • 3518 Views
  • 7 replies
  • 0 kudos

Resolved! STM32L0 current consumption jumps from 650uA to 2-8mA

Hi,I'm working on a low power project that my micro-controller can only have 1mA in 2.7V.My micro-controller is stm32l051c8 and its works nice with its peripherals (ADC and Timer) and its current consumption is about 0.65 mA. But After working for A ...

sshaf.1 by Associate
  • 2073 Views
  • 4 replies
  • 1 kudos

STM32 I2C not receiving further bytes

Hello I am beginner to MCU, I have set STM32F407 Discovery as a master on I2C communication with nucleo STM32F446RE as a slave. PC host connected to the STM32F407 via UART. The code for the master ischar RecBuff [20]; while (1) { HAL_UART_Receiv...

0693W000005BNhPQAW.jpg
HGhaf.1 by Associate
  • 934 Views
  • 1 replies
  • 0 kudos

STM32H743ZI Nucleo 144, UART interrupt handling

Hello ST family, I'm working on STM32H743ZI chip for my project. I want to execute simple program which communicates with PC through RS232 UART with configuration of 9600 baud rate, 1 stop bit and no parity and No Fifo used. Functionality should be s...

Manju by Associate II
  • 871 Views
  • 0 replies
  • 0 kudos

Need help getting 1.8V SD card working on STM32H743

I have a new board design that interfaces an STM32H743 to a uSD card using 1.8V I/O. The SD Card is powered by 3.3V, and the card I am using supports the LVS mode of SD. I'm having a hard time trying to get the card up and running, and my searche...

JDell.3 by Associate
  • 1549 Views
  • 2 replies
  • 1 kudos

SDRAM W9812G6KH and STM32H732

Hello!​I have never created custom PCB with SDRAM before and I would like to clarify whether this memory will work with FMC.​Thank you very much!​

AKosi.1 by Associate
  • 1071 Views
  • 0 replies
  • 0 kudos