STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How should I use argument "Channel" in function: HAL_SDADC_InjectedGetValue(SDADC_HandleTypeDef *hsdadc, uint32_t* Channel)

Hi!I'm trying to make 16-bit ADC measurement works but I have some trouble understanding the argument Channel. First I have these SD-ADC channels.SDADC1 have:IN4 = Single zero referenceIN6 = DifferentialIN8 = DifferentialSDADC3 have:IN6 = Single zero...

0693W000006EzhIQAS.png 0693W000006GXNdQAO.png
DMårt by Lead
  • 989 Views
  • 0 replies
  • 0 kudos

How can I use audio on STM32F7508-DK board ? There is a WM8994 connected to SAI2, but I couldn't find any example of audio using SAI, neither audio example for this board. And the driver for the WM8994 is not provided.

I watched many examples on other boards, but they are always using I2S so I couldn't transposate to my case (SAI).For now, I just would like to connect inputs (Jack IN1 or mems microphone IN2) to the output to understand how it works (maybe first via...

PDand.2 by Associate
  • 765 Views
  • 0 replies
  • 0 kudos

STM429I-EVAL1 Joystick Interrupt by ISR

Hello,I am using a STM429I-EVAL1 board. With this I try to trigger an interrupt by pressing on the joystick, which is on the board. The interrupt is executed correctly a few times, but then it aborts. You can't tell when, it can abort after the 10 ti...

OBorz.1 by Associate II
  • 1419 Views
  • 2 replies
  • 0 kudos

Resolved! STM32L011K4 - Configuring PC14 and PC15 as GPIO outputs?

From the STM32L011K4 datasheet, it appears PC14 and PC15 can be used as GPIO outputs as long as OSC32 is not used. Has anyone else done this before? I'd like to drive two LEDs at 3.3V, trying to make a simple sample program to confirm if this is poss...

ZRatt.1 by Associate II
  • 4151 Views
  • 4 replies
  • 0 kudos

Keeping PA15 low during the init

Hi community,I'm using STM32F303RE, in that I'm using PA15 as a GPIO which is connected to a Relay, but I recently found out that the PA15 is a JTDI pin which is being pulled up internally, so whenever the STM32 resets, it gets high and after GPIO_in...

Reboot necessary after OTP write?

I am using the STM32L432KCU for a project. I intend to use the OTP area for writing persistent device information (serial number, encryption keys, etc).Is a reboot necessary after writing to the OTP area?Can the OTP region be written to 32 bits at a ...

some question about DALI Slave in STM32F

DALI_RX port and DALI_TX port have been initiated twice in" void DALI_Init(TDLightControlCallback LightControlFunction) " and "init_DALI(OUT_DALI_PORT, OUT_DALI_PIN, INVERT_OUT_DALI, IN_DALI_PORT, IN_DALI_PIN, INVERT_IN_DALI, DALI_Interrupt, DALI_Err...

0693W000003P8hPQAS.png 0693W000003P8e6QAC.png
晓石.1 by Associate II
  • 1620 Views
  • 3 replies
  • 0 kudos