STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G070RB, Maximum Alarm length

What is the maximum alarm length in the G070. I only see about 30days.I need 6 months.I guess I could implement one using the TAMP_BKPxR registers and compare the RTC DR , TR with the alarm values I have store in the TAMP regs. ( stripping out the W...

MEder by Associate III
  • 1495 Views
  • 3 replies
  • 0 kudos

STM32H743 Nucleo board SEGGER JLink issue

Hi There, I bought two STM32H743 Nucleo boards recently and did some tests on them. As usual, I first converted ST-Link v2 to JLink interface using the tool SEGGER provided. I have done this with F1, F4, and F7 series boards in order to use JLink RTT...

XZ by Associate II
  • 9177 Views
  • 20 replies
  • 0 kudos

SysTick timer registers give an error when called

Hi , i checked the registers for the system clock and i found these registers , but they dont seem to worki , insead , i have to use systick->CTRL , but i cant find the definition from thwere the syntax comes from

0693W000007D2xEQAS.png 0693W000007D2x4QAC.png
AMat.1 by Associate II
  • 713 Views
  • 1 replies
  • 0 kudos

TIMER with DMA call back function

Hi,void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim){ if(htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1) {  captureDone = 1; }}HAL_TIM_IC_Start_DMA(&htim2, TIM_CHANNEL_1, (uint32_t*) captures, 2);void HAL_TIM_IC_MspInit(TIM_HandleTypeDef* htim_ic){...

NPULI.1 by Associate II
  • 2148 Views
  • 1 replies
  • 0 kudos

STM32H723 Interface with QuadSPI flash

Hi everyone,for the first time i'm trying to interface my micro H7 to a Macronix QSPI Flash.Micro Model : ST32H723Flash Model : MX25L3233FM1I.These are the instructions that I do:read status register in order to verify QUAD ENABLE (OK)If not QUAD ENA...

MDell.1 by Associate II
  • 2590 Views
  • 0 replies
  • 0 kudos