STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Independent watchdog timer makes my MCU unstable

Hello,Here is my source code:  void WatchDog(void){   NVIC_InitTypeDef nvicStructure; NVIC_PriorityGroupConfig(NVIC_PriorityGroup_2);   nvicStructure.NVIC_IRQChannel = WWDG_IRQn; nvicStructure.NVIC_IRQChannelPreemptionPriority = 1; nvicSt...

JJohn.3 by Associate II
  • 644 Views
  • 0 replies
  • 0 kudos

I'm about to start embedded programming and have an STM32f103C8T6 ARM-Coretex-M3 board to get started with. I'm also a C++ programmer and want to use that language to program a project to blink the LED of that board as my first embedded task.

Hi all, Apart from the board and two machines (Windows and Linux) I have also an MB-102 breadboard and a bunch of cables in hands. Firstly I wanted to make use of this tutorial for the task above but it's dealing with NUCLEO-L476RG that I lack for th...

Adev.1 by Associate III
  • 1856 Views
  • 3 replies
  • 0 kudos

I missed the confirmation E-Mail for the session.

Hello ST.I have missed the confirmation mail but I do pretend to join the session.My Board's buy is handled be my company's sales and should be invited soon.Please add my to the 11/3 session again.Thanks,Hagay

HHali.1 by Associate
  • 1089 Views
  • 1 replies
  • 0 kudos

DMA UART TX single transfer

Hello, I have an stm32F103, I would like to start using DMA to transfer data from memory to TX pin, in circular mode it works fine but when I switch to normal mode it works only once, I cannot use the debug function since I'm not using a ST-Link, so ...

Vertinhol by Associate III
  • 1874 Views
  • 2 replies
  • 0 kudos

Resolved! USB CDC does not work when I unplug and replug STM32

I'm using the Nucleo-H743ZI STM32 development board on windows 10. When I upload a program that sends out data through CDC with CDC_Transmit_FS and open a serial monitor right after, it works fine. But when I disconnect and reconnect the Nucleo to my...

csotiriou by Associate II
  • 1660 Views
  • 1 replies
  • 0 kudos

STM32 Timer auto-reload preload

The conditions to reproduce: Here is my real life example that I would like to solve:I am developing an application on an stm32f411RET which needs to dynamically change the period of two PWM's.The two PWM's need to be synced and have exactly the sam...

SMour.1 by Associate III
  • 8403 Views
  • 7 replies
  • 2 kudos