2020-11-04 10:29 AM
hi there
I want to concatenate these 2 byte arrays
uint8_t START_BYTE[2]={0x05,0x64};and
uint8_t disunsini[]={0x15,0x3C,0x02,0x06,0x3C,0x03,0x06,0x3C,0x04,0x06};so I can get
{0x05,0x64,0x15,0x3C,0x02,0x06,0x3C,0x03,0x06,0x3C,0x04,0x06};I used the code below
temp=(START_BYTE<<8)|disunsini;but I get the error
INVALID OPERANDS TO BINARY EXPRESSION (UINT8_T * (AKA UNSIGHED CHAR*) AND INT)
why is that?
Solved! Go to Solution.
2020-11-04 11:19 AM
There're many correct ways. Every way varies, e.g. its number of cycles for the processor to execute, its size of code, its size of data, etc. This is the simplest way, using the standard library function memcpy:
#include <stdint.h>
#include <string.h>
int main(void)
{
uint8_t START_BYTE[2]={0x05,0x64};
uint8_t disunsini[]={0x15,0x3C,0x02,0x06,0x3C,0x03,0x06,0x3C,0x04,0x06};
uint8_t concatBuf[sizeof(START_BYTE) + sizeof(disunsini)];
/* Copy START_BYTE to the start of concatBuf */
memcpy(concatBuf, START_BYTE, sizeof(START_BYTE));
/* Copy disunsini to the byte position following it */
memcpy(concatBuf + sizeof(START_BYTE), disunsini, sizeof(disunsini));I found these on Google to explain your mistake and the operation of memcpy:
https://www.tutorialspoint.com/cprogramming/c_bitwise_operators.htm
https://www.tutorialspoint.com/c_standard_library/c_function_memcpy.htm
2020-11-04 11:19 AM
There're many correct ways. Every way varies, e.g. its number of cycles for the processor to execute, its size of code, its size of data, etc. This is the simplest way, using the standard library function memcpy:
#include <stdint.h>
#include <string.h>
int main(void)
{
uint8_t START_BYTE[2]={0x05,0x64};
uint8_t disunsini[]={0x15,0x3C,0x02,0x06,0x3C,0x03,0x06,0x3C,0x04,0x06};
uint8_t concatBuf[sizeof(START_BYTE) + sizeof(disunsini)];
/* Copy START_BYTE to the start of concatBuf */
memcpy(concatBuf, START_BYTE, sizeof(START_BYTE));
/* Copy disunsini to the byte position following it */
memcpy(concatBuf + sizeof(START_BYTE), disunsini, sizeof(disunsini));I found these on Google to explain your mistake and the operation of memcpy:
https://www.tutorialspoint.com/cprogramming/c_bitwise_operators.htm
https://www.tutorialspoint.com/c_standard_library/c_function_memcpy.htm