STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! how to jump out of while()?

hey thereI have the code belowuint32_t startTime = HAL_GetTick(); while (HAL_GetTick() - startTime < 5000) { for (int i = 0; i < 3; i++) { if (strstr(InputMSG, answerSearch[i])) { resault = 1; break; } } }wh...

Ala by Senior
  • 1445 Views
  • 2 replies
  • 0 kudos

Resolved! STM32G0B1 release date and compatibility

HiCurrently we are using the STM32G071 MCU, but we will running out of flash memory soon, so we looking for an alternative. I've seen that a bigger G0x1 (STM32G0B1) will be available in the second half of this year. Are there more details available f...

Marco.R by Senior
  • 3575 Views
  • 5 replies
  • 0 kudos

Interface CAN with STM32f4 and STM32f091

HII am trying to interface Stm32f407board with cjmcu2551 transceiver with tcan1051V module and stm32f091cct6.the clock rate for both controllers(APB1 for CAN=25Mhz) with prescalar=5, time segment1=8 and time segment 2=1 with baud rate 500kbps. i am n...

PJose.1 by Associate II
  • 1930 Views
  • 3 replies
  • 0 kudos

Does ADC regular conversion in DMA mode and ADC injected conversion in interrupt mode work together using HAL driver? STM32F303

Hello,I have 6 ADC channels that shall be launched by software in regular conversion mode. I set the ADC to "End of sequence" and enabled DMA to jump into the callback function when all channels are converted. This is working fine so far.I have anoth...

Markus11 by Associate
  • 923 Views
  • 0 replies
  • 0 kudos

OSPI Flashing in IAR EWARM

Hello,I am working on a project that wants to store pre-built binary files in the OSPI on the STM32L562E-DK. I am using all of the default jumper settings for the board. When I build my project in IAR EWARM 8.50.9 and then try to program the device v...

IFyal.1 by Associate
  • 1285 Views
  • 1 replies
  • 0 kudos

How to redirect std::cout to ITM port 0

Hi everyone, I have successfully used the following code to redirect the printf output to SWD, ITM View/* USER CODE BEGIN 4 */ int __io_putchar(int ch) { ITM_SendChar(ch); return ch; } /* USER CODE END 4 */Now I am working with C++ and would...

Xxoyo.1 by Associate III
  • 965 Views
  • 0 replies
  • 0 kudos