STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to receive the data from SIM39EA Gps module?

I'm interfacing stm32f series microcontroller and SIM39EA gps module Thruogh terminal im getting this data but not valid data. /**************************************/$GPGSA,A,1,,,,,,,,,,,,,,,*1E$GPGSV,1,1,04,13,,,26,05,,,21,12,,,19,02,,,19*7C$GPRM...

MVENN.1 by Associate II
  • 795 Views
  • 0 replies
  • 0 kudos

STM32F7 How to design external oscillator

Hello,I have been trying for a while now to properly design the external oscillator for the STM32F722RE MCU.Until now, I don't find a clear answer with detail calcul.To design the oscillator, I use 3 documentations:stm32f722re.pdfcd00221665.pdf (AN28...

0693W000007ZLw9QAG.png 0693W000007ZLy0QAG.png 0693W000007ZLrAQAW.png 0693W000007ZLzSQAW.png
BSchn.2 by Associate II
  • 2471 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F373 SDADC Analog input range

Hi, I have 50Hz sinewave with 660mVp-pk, should i connect this to SDADC analog input? It can measure negative cycle of the sinewave? i.e. If i configure SDADC as single ended zero reference mode then it can measure negative cycle of the sinewave?Na...

16 Bit SDADC is only giving 15 Bit value

I am running both SDADCs on a STM32373C-EVAL evaluation board. One of them is giving me the correct values from 0-65.535 but the second one is giving me 0-32.767 on the same voltage.I have configured them using the Cube IDE and Hal. They are set up e...

RKage.3 by Associate
  • 1105 Views
  • 1 replies
  • 0 kudos

Resolved! Fully compatible migration from STM32F745VG to STM32F765VI ?

Hello,For a project I am running code on STM32F745VG. I would like to migrate and replace this MCU with a STM32F765VI with more Flash memory (2MB instead of 1MB). I saw that these two MCUs are pin to pin compatible, but do I need to modify my hardwar...

VPerr.1 by Associate
  • 2121 Views
  • 3 replies
  • 0 kudos

Few questions about STM32 microcontrollers

Hello, I have a few questions about STM32 microcontrollers: I want to create a personalized card and use CAN, RS485, I / O, ... to connect several devicesI need an HMI to control the controller (touchgfx? Or Visual studio?)I want a clear program (mai...

KMiko.1 by Associate III
  • 6107 Views
  • 14 replies
  • 1 kudos

Wake up Pin from standby mode

I am using wake up PIN1 (PA0) to wake the STM32F746 from standby mode. I have PA0 connected to a push button with a pull down resistor. When first powered up the MCU goes into standby mode and stays in it until I press the button connected to PA0. T...

Nano second Precision using a hardware timer on STM32L4S5ZI

Hi,I am working with STM32L4S5ZI MCU and I have a custom board with the same.I am evaluating the hardware timer and as part of my project I need time in nano seconds for some time constrained work. Right now I am using Timer3 and below is my sample c...

SJant.1 by Associate III
  • 6536 Views
  • 17 replies
  • 0 kudos