User Activity

I got a project with a flex button in screen and custom container with the same name ("ButtonBack"). Both flex buttons got an action to call a virtual function. After generate, close TouchGFX Designer and reopen, the reference button in action is mis...
Hello,I'm trying to use a Scrollwheel inside in a Scrollable Container, but, the Scrollwheel don't recognize click events or draggable events. Is it possible to work both components together?
I'm trying to use images through the flex button, but, when i select some images, there isn't any visual update and selection update. I tried change the "released" image and continuous with "No image" after the selection in my library images.anyone k...
I need to know X and Y position from some points in static graph widget. Is it possible to getX and getY from the vector datapoint of static graph?
I have updated from stm32cube IDE 1.10.1 to 1.11.0 . After update and open the .ioc file, clock configuration show some problem like the CPU max clock frequency i can't use 480MHz any more. Do you know anything about this bug?The H7 Package in CubeMX...
Kudos from