STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What Xferoption should be selected in SMBUS for restart condition?What is Xferoption for restart condition with change in direction(write to read)?

/* List of XferOptions in usage of : * 1- Restart condition when direction change * 2- No Restart condition in other use cases */#define SMBUS_FIRST_FRAME      SMBUS_SOFTEND_MODE#define SMBUS_NEXT_FRAME     ((uint32_t(SMBUS_RELOAD_MODE|SMBUS_SOFTEND_...

VKamb.1 by Associate
  • 1056 Views
  • 0 replies
  • 0 kudos

Resolved! stm32f2xx flash erase as painfull as it looks?

I am porting some code from stm32f105 to stm32f205.stm32f105´s memory is erased in 64 pages of 2kbytes (i can handle this)stm32f205´s memory is erased in 12 sectors of 42kbytes!!? (flash size is 512kB)(from stm32f2xx_hal_flash_ex.h)/** @defgroup FLAS...

Javier1 by Principal
  • 1971 Views
  • 3 replies
  • 0 kudos

Resolved! Which is the maximum sampling frequency of ADC? STM32H742

I am trying to configure STM32H742 to convert 3 different input channels (3, 5, 16) in an ADC (1) . I have achieved to convert just one channel with a sampling frequency of 1MHz, seeing that 1 million samples are converted per second. But when I add ...

EEtxe.1 by Associate II
  • 1709 Views
  • 2 replies
  • 0 kudos

RM0091 - ADC chapter not very clear

Hi,The RM0091 rev 9 has some contradictions and typos in the ADC chapter.on page 234, 13.4.4 says that the registers IER, CFGRi, SMPR, TR, CHSELR and CCR must be configured only after ADEN has been set (and presumably that ADRDY is also set).However ...

Kraal by Lead
  • 2248 Views
  • 7 replies
  • 1 kudos

How G-431B-ESC1 drives CAN & PWM communication?

Hello ST,I bought a G-431B-ESC1, wish to driven with CAN & PWM, but cannot figure it out . I red the manual(UM2516) was written:"The CAN interface is provided with transceiver on board and a termination resistor is provided and manageable by firmware...

GST by Associate
  • 1096 Views
  • 1 replies
  • 0 kudos

Resolved! SPI CPHA affects NSS

I use MCU STM32L462ET6TR. When I set CPHA=1, the NSS signal is always at low. When CPHA=0, NSS signal works normally. There is my initialization code:void MX_SPI1_Init(void) { hspi1.Instance = SPI1; hspi1.Init.Mode = SPI_MODE_MASTER; hspi1.Init...

sdianoff by Associate II
  • 2138 Views
  • 3 replies
  • 0 kudos

stm32f103c8t6 suggest for new design?

Hi there, since Nov. 2020, we have placed some orders to Arrow China, but till now, no one package received, and even no any upate about the orde. ​Please help us with current situation, we start use ST processor since 2010, but now... really sad a...

Xmiao.1 by Associate
  • 1018 Views
  • 1 replies
  • 0 kudos

Resolved! USART3 (PB10, PB11) not working on NUCLEO-G474RE

Hello,I'm working on a NUCLEO-G474RE board (using the LL libraries available on ST site), and I came across an issue, the USART3 available on the PB10 and PB11 is not working. I tried to generate the same code from the CUBEMX as well but unfortunatel...

0693W000008GNhlQAG.png