STM32 Firmware Compatible Suffixes
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-11-26 6:03 AM
Which suffixes can share the same elf file or bootloaded app binary?
- Likely Temperature range has no effect on firmware load?
- Will changing only the package type affect firmware load? (LQFP, BGA, CSP ...)
- Will changing only the number of pins affect firmware load? (64, 100, 132...)
(assuming keep same function on matching port pin of new package).
- Will change in memory size affect firmware load, or is there a way to retain compatibility?
(This is only needed for bootloaded code, option bytes won't change)
======== Details ========
For elf file and/or bootloaded apps are any other parts compatible with:
- STM32L4A6VGT6 (Has features needed by most remotes)
maybe some firmware load compatibility:
RGT6=1MB/320KB, 85'C, LQFP64,
VGT6=1MB/320KB, 85'C, LQFP100
VGY6=1MB/320KB, 85'C, WLCSP100
QGI6=1MB/320KB, 85'C, UFBGA132
ZGT6=1MB/320KB, 85'C, LQFP144
AGI6=1MB/320KB, 85'C, UFBGA169
- STM32H743BIT6 (Chosen as STM with most ADC channels)
maybe some firmware load compatibility:
VIT6 =2MB/1MB, 85'C, LQFP100
VIH6=2MB/1MB, 85'C, TFBGA100
ZIT6=2MB/1MB, 85'C, LQFP144
AII6=2MB/1MB, 85'C, UFBGA169
IIT6=2MB/1MB, 85'C, LQFP176
BIT6=2MB/1MB, 85'C, LQFP208
?IK6=2MB/1MB, 85'C, UFBGA176+25
?IH6=2MB/1MB, 85'C, TFBGA240+25
Purpose is a network of remote modules
- Firmware update by RS485 custom bootloader from SD card or USB stick at central location.
- hopefully sharing as few firmware loads as possible across different but compatible PCBs.
- most remotes cost&size minimized where reasonable.
- some remotes needing more features and thus more pins and memory (ADCs, LCD...).
Paul
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-12-15 1:46 PM
Answer from Support Ticket:
- In same series (same ss in STM32ss) then if peripherals exist they will be at same address (i.e. CAN2 at same address in chips of the series).
- As long as ensure only access existing memory and peripherals then ELF will be compatible within a series (and you can bootload ELF or binary).
- (Peripherals may be at different addresses in different series).
- (Changing Option bytes may require special attention, see AN3155 https://www.st.com/resource/en/application_note/cd00264342-usart-protocol-used-in-the-stm32-bootloader-stmicroelectronics.pdf)
Paul