cancel
Showing results for 
Search instead for 
Did you mean: 

How do i read the response from Quctel M66 via UART on putty? I am using nucleo 32 controller.

NHing.1
Associate III
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

You'd need to determine the UART connected to the VCP and that used by​ the modem, and then forward the data between the two.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

2 REPLIES 2

You'd need to determine the UART connected to the VCP and that used by​ the modem, and then forward the data between the two.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

I changed the rx pin of controller from pin 15 to D4/A7

so that i am able to connect tx of mc66 to rx of controller.