STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

F042 ADC DMA malfunction:?? I am using a Nucleo_F042k board but will target a F042F MCU later. I'm using DMA to set up 2 ADC channels + the 3 internal ADC values. Results : 1: 2146: 2: 1668: 3: 0: 4: 0: 5: 0. Only the first is verifiable.

I have probably missed something simple. I use CubeMx to Configure the A2D channels hadc.Instance = ADC1; hadc.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1; hadc.Init.Resolution = ADC_RESOLUTION_12B; hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT; ...

DIngr.1 by Associate II
  • 1263 Views
  • 1 replies
  • 0 kudos

about dominant error

Dear Guys I get the "bit dominant error" when programming for can with STM32F302. even i set CAN_MODE_SILENT_LOOPBACK mode , also get this error after exec the statement  "SET_BIT(hcan->Instance->sTxMailBox[transmitmailbox].TIR, CAN_TI0R_TXRQ);" a...

0693W00000BZZg1QAH.png 0693W00000BZZfhQAH.png
kevin xu by Associate II
  • 1602 Views
  • 2 replies
  • 0 kudos

Wrong data through SPI on STM32F7

Hello dear community. I'd tried so long so i decided to ask for you.I need to send some data pack from STM32F7(master) to STM32F1.I use STM32CubeIDE platform. My code is below.Problem is that in receiving back data by master. First byte has always co...

DVovk.1 by Associate II
  • 15885 Views
  • 14 replies
  • 0 kudos

HardFault went reading flash

This routeen fails on the lineFlash_End_Address() at flash_page.c:87 0x80004e6where line 87 is *DATA_64 = *(__IO uint64_t *)StartPageAddress;_______________________________________________________________________________________uint32_t Flash_End_Add...

PGood.1 by Associate II
  • 690 Views
  • 1 replies
  • 0 kudos

Hello every one I have problems with the ISM43362-M3G-L44 module to receive messages from a mqtt broker. Can somebody help me?

I am writing a library for the ISM43362-M3G-L44 module of the B-L475E-IOT01A, and I have a problem with receiving messages from an MQTT broker, when I ask the first time it works correctly but after the module stops responding , it no longer accepts ...

JArra.1 by Associate
  • 778 Views
  • 0 replies
  • 0 kudos