User Activity

Hello,We have purchased the STM32F769I-DISCO KIT as we plan to use STM32F769I in USB audio IN/OUT application.I am trying to make "STM32CubeExpansion_USBAudioStreaming_V1.0.0" example provided by ST working. So far: I have configured the above exampl...
Hello,I have an interrupt driven I2C which is working fine. I know that this is not very clean design but I need to execute few I2C transactions from a button interrupt handler (EXTI9_5_IRQn). I have set the priority of the EXTI9_5_IRQn 1 and the pri...
Hello We need to interface TDM bus with USB from i7 based embedded PC. I saw "STM32 USB Device Audio Streaming software expansion for STM32Cube" and I am consider using it. Let me put here our requirement, possibly someone can comment if what we need...
Posted on September 27, 2016 at 14:48Hello,I am using STM32Cube_FW_L4_V1.5.1 library and I am trying to test the STM32Cube_FW_L4_V1.5.0\Projects\STM32L476G_EVAL\Applications\USB_Device\DFU_Standalone application. I have STM32L476RG-Nucleo + NUCLEO-C...
Kudos from