STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ads124s08 with STM32F407VGT6 spi communication problem

I need to get information from an ti's ads124s08 and imported an example from arduino forums. I can communicate with device using an arduino for test (on the same board and same specs) but can not use with stm. In fact, i think there should be a prob...

TBala.1 by Associate
  • 3078 Views
  • 2 replies
  • 0 kudos

Self-generated breaks are not detected sometimes

We configured our controller (STM32F427IG) as master and USART8 to LIN-mode. We observed, that the own breaks are detected with the break detection interrupt. Furthermore, we also get the framing error interrupt as the stop bit arrives later for the ...

0693W00000BZxSIQA1.png
TGnäg.1 by Associate II
  • 3580 Views
  • 7 replies
  • 0 kudos

Resolved! Generate Noise Using LFSR (Linear Feedback Shift Register)

Hello,I am trying to generate white noise using the DAC, much like was mentioned in this forum post:How to generate a white noise with the DAC on STM32L1However, I don't know if putting values into memory table and using cyclic mode is the only answe...

0693W00000BZsRtQAL.png 0693W00000BZsT6QAL.png 0693W00000BZsT7QAL.jpg

stm32f4 using NVIC_SystemReset() fails to reset

Hello,My board consists of stm32f427 and I have a strange problem.Calling NVIC_SystemReset() causes CPU to hang. This happens only on some boards.I could overcome the problem in one of the following:Add a HAL_Delay(100) before calling NVIC_SystemRese...

ari_v2 by Senior
  • 16172 Views
  • 11 replies
  • 0 kudos

How to determine what type of FIR filter is being used?

I am reviewing another person's program and need to know how the filters are operating for troubleshooting. Here are a few examples from the program I am looking at.filter_arm_status = arm_fir_decimate_init_q15(&Sine_Filter, 31, 2, FIR_Coeff_Buffer, ...

DeBoots by Associate
  • 1049 Views
  • 1 replies
  • 0 kudos

STM32H7 SRAM ECC or STL ram tests to achieve DC up above 90%?

HI ! There is a functional safety program when uesd STM32H750, I notice this MCU have ECC in SRAM part,。 so , If I only used ECC function , can I get 90% DC rate? And why in STM32H7 STL lib still have RAM TESTS lib and not used ECC instead?Thanks...

Ccl.1 by Associate
  • 587 Views
  • 0 replies
  • 0 kudos