cancel
Showing results for 
Search instead for 
Did you mean: 

Measurement of current consumption in MCU

HNdal
Associate III

I have a Nucleo 64 STM32F303RE, I would like to measure the current consumed by the MCU while running application. How do I do it ?

This discussion is locked. Please start a new topic to ask your question.
7 REPLIES 7
KnarfB
Super User

Check the UM1724 User manual STM32 Nucleo-64 boards. There are schematics at the end. Measure the current at JP6.

Yes thank you,one more thing,

I supposed this can be done with the board supplied by USB?,

In this case , the voltage supplied to MCU will be measured between VDD and ground.

Ozone
Principal III

> I supposed this can be done with the board supplied by USB?,

Yes.

I suggest to additionally consult the schematics, to see where you measure, and what.

HNdal
Associate III

Thank you so much.

Mohamed Aymen HZAMI
ST Employee

Hello @HNdal​ ,

You can measure the current consumption on the IDD JP6 jumper.

Best Regards,

Mohamed Aymen.

Thank you so much, and the voltage accross the MCU would be between VDD and VSS pins?

right.