STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7 SRAM ECC or STL ram tests to achieve DC up above 90%?

HI ! There is a functional safety program when uesd STM32H750, I notice this MCU have ECC in SRAM part,。 so , If I only used ECC function , can I get 90% DC rate? And why in STM32H7 STL lib still have RAM TESTS lib and not used ECC instead?Thanks...

Ccl.1 by Associate
  • 587 Views
  • 0 replies
  • 0 kudos

Resolved! MCU crashes after using HAL_OB function.

I have tried the HAL_OB function.No change was good.So I ran the code below.After that, ST LINK connection is not possible.MCU is not responding.Is there no way to get it back?MCU : STM32G07xCODE :         FLASH_OBProgramInitTypeDef OBInit;        if...

ckim.2390 by Associate II
  • 1210 Views
  • 1 replies
  • 0 kudos

Error while connecting g070rb

When i try to connect g070rb nucleo board i get my LD1 blinking continuously and on my pc it shows usb device not detected​.

AVerm.4 by Associate III
  • 2144 Views
  • 3 replies
  • 0 kudos

About STM32 Network library TCP disconnect problem

Recently I ran into a problem with data loss when TCP was disconnected。​I used Keil's official Network librarynetTCP_SendReady is unable to immediately detect that the TCP has been disconnected, resulting in data loss issues​Is there a way to speed u...

0693W00000BZxVHQA1.png
YZHIL.1 by Associate
  • 906 Views
  • 0 replies
  • 1 kudos

How to form Can Remote request Frame?

i want to know how to form Remote Request (frame) to get the data from host device.Is only two settings are enough (RTR bit set to CAN_RTR_REMOTE & data length = 0) suggest the whole configuration to get the data from host device.Controller suppose ...

Ss.61 by Associate III
  • 1011 Views
  • 0 replies
  • 0 kudos

eMMC 5.1 / STM32F4 Compatible?

Posted on January 23, 2018 at 19:55We are looking to replace an eMMC 4.41 chip (by Micron) that we currently use with a new one SanDisk iNAND 7250-I (https://media.digikey.com/pdf/Data%20Sheets/Micron%20Technology%20Inc%20PDFs/EMMC_Series.pdf). This...

Craig B by Associate II
  • 8304 Views
  • 12 replies
  • 0 kudos