STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to excess DMA_SxNDTR register

I am trying to collect data from ADC using DMA in circular buffer mode.i want to excess/read DMA_SxNDTR register. also tell me how to read data from circular buffer. I have written code for reading count from DMA_SxNDTR but it is not working , it is...

0693W00000Bb9ZrQAJ.jpg
NKann.1 by Associate III
  • 1787 Views
  • 5 replies
  • 0 kudos

STM32G4 ADC1 DMA issue.

I am trying to read 3 ADC channels (ADC1) via DMA but I get false values in the watch window./* Private user code ---------------------------------------------------------*//* USER CODE BEGIN 0 */uint32_t value1[3];/* USER CODE END 0 *//** * @brief T...

PGand by Associate
  • 1086 Views
  • 1 replies
  • 0 kudos

Yet another "No ST-LINK detected! " issue

I have had STM32CubeIDE v1.3.0 working with my hardware. I just upgraded to Cube to v1.6.1. Now when I try to debug, I get "No ST-LINK detected! " message box This has happened before (my upgrade to 1.4.1 failed so I rolled back to 1.3.0). ST-LINK...

RWeil.3 by Associate II
  • 2260 Views
  • 5 replies
  • 0 kudos

Failed to communicate with device using Nucleo uart

Hello,I'm using nucleo board f410rb to communicate with another device via UART, my Baudrate is correctly fixed , i checked with the builder of the device the command i should send , i wrote the following code but the device dosen't respond uint8_t t...

Ahajr.1 by Associate II
  • 1325 Views
  • 1 replies
  • 0 kudos

Resolved! Translating incoming data from PA10 (USART1 Rx) to PB4 (JTRST) with erased FLASH or under reset in STM32G473

I have RS-485 transceiver connected to USART1 (PA9 + PA10) and relay connected to PB4. If MCU have erased FLASH or RST-pin connected to GND all incoming data to pin PA10 (Rx) for RS-485 line translated to pin PB4 in inversion (0 on PA10 => 1 on PB4, ...

Nabekaite by Associate II
  • 3389 Views
  • 8 replies
  • 0 kudos

Not able to program STM32F407G-DISC1 via onboard ST-LINK. In STM32CubeProgrammer Target voltage is detected as 0.

I purchased a new STM32F407G-DISC1 (MB 997D) board last week. As shown in many of the videos, I am not able to program it using STM32CubeIDE. Tried with ST-Link utility & STM32CubeProgrammer as well but no luck. I observed target voltage is detected ...

nilesh-g by Associate
  • 1552 Views
  • 2 replies
  • 0 kudos

STM32L412 and reference voltage buffer

STM32L412xx datasheet DS12469 even in Rev. 8 talks about � Accurate 2.5 V or 2.048 V reference voltage buffered outputon the front page. The reference manual gives only availability on L43 and L45.