Skip to main content
ABous.3
Associate II
February 10, 2021
Solved

HardFaults at random places in code on an STM32F722

  • February 10, 2021
  • 12 replies
  • 3156 views

Hello,

I am facing random HardFaults on a STM32F722. They happen at various places in code, sometimes even during stack's initialization.

Stack's analysis do not show any risk of overflow : most of the time, the problem happens while executing main() loop, and stack's width is never more than 2 levels.

Looking at Fault status Registers shows:

_ bit FORCED of HFSR is set to 1

_ CFSR = 0x1000000 = bit UNALIGNED of UFSR set to 1: unaligned memory access. 

bit UNALIGNED_TRAP is set to 0

Looking around PC and LR, I only see "unoffensive" instructions (typically, ldr, str, or ldr.b and str.b), and the code registered in stack is part of my main's infinite loop, which most of the time executes without any trouble. So I do not understand how it could sometimes trigger a memory alignment fault...!

I read https://community.arm.com/developer/ip-products/processors/f/cortex-m-forum/43707/unable-to-determine-offending-instruction-usage-fault-illegal-unaligned-load-or-store-cortex-m7-keil-mdk-pro, and the associated links, but did not find what could trigger this fault on my board.

One track that seemed interesting was https://www.keil.com/support/docs/3777.htm, but I am not using an external SDRAM...

I also saw the following topic, which seems to be exactly the same issue than mine: https://community.st.com/s/question/0D50X00009XkiJw/stm32f7-hardfault-unaligned-memory-access?t=1612969638024. But my HCLK is at 16 MHz, so, according to STLM32F7xx's reference manual, the only latency that I can use for flash accesses is 0 WS, which is already the case...

I am using HAL for startup code and basic (while(1)) fault handlers (so I do not understand why my UsageFault escalated to HardFault, as UsageFault handler is pressent in my code).

I am using gcc and gdb with Atollic TrueStudio as IDE.

Can you please help me to solve this issue?

Regards

This topic has been closed for replies.
Best answer by ABous.3

Hi everyone,

Thank you for your advices.

On friday my colleague saw that some capacitors were missing on my board, and corrected this. My board has been running for the weekend, and no hardfault happened. I am leaving it running a longer time to ensure this was not luck. I also flashed another board with my software and will let it run.

I will keep you informed.

Have a nice week!

Best regards

12 replies

Uwe Bonnes
Chief
February 10, 2021

Too high frequency, to few wait states and a flacky supply are first points to look at.

ABous.3
ABous.3Author
Associate II
February 11, 2021

Hi Uwe,

Thank you for your response.

My CPU is running at 16 MHz. This is the lowest frequency I can set on my hardware, and at this speed, STM32F7xx's reference manual gives choice between 0 WS and 0 WS for flash latency.

Concerning power supply, my hardware's colleague did not see any problem on the past

Piranha
Principal III
February 10, 2021

What is the initialization value of the stack pointer? Is it valid and 8-byte aligned?

Are the compiler and runtime library FPU settings appropriate?

ABous.3
ABous.3Author
Associate II
February 11, 2021

Hi Piranha,

Thank you for your response.

My stack pointer is initialized at 0x20040000, so perfectly aligned.

As I am not using floating points in my code, I tried to disable FPU in my compiler's settings (it was enabled previously). For the moment the fault has not appeared, but as it is triggered very randomly, maybe this is just a matter of luck...

Piranha
Principal III
February 11, 2021

Just in case...

Note that the hard-float and soft-float ABIs are not link-compatible; you must compile your entire program with the same ABI, and link with a compatible set of libraries.

https://gcc.gnu.org/onlinedocs/gcc/ARM-Options.html

Therefore disabling FPU with -mfpu option (or adding +nofp to -march or -mcpu) also requires setting -mfloat-abi=soft.

Uwe Bonnes
Chief
February 11, 2021

Strip down the program to the bare minimum showing the problem. Port to a known working F722 board and test there.

Tesla DeLorean
Guru
February 11, 2021

+1 known hardware

If problem not software, look at hardware issues.

Check voltage and capacitors placed on VCAP pin(s)

The F722 uses a newer ARM core than the F746

Use a Hard Fault handler that dumps the register, not sure what you've got, not showing a full register set and stack top here.

Could double fault if stack at wrong address. Check for corruption.

Random faults, need to be looking at interrupts. SysTick, others..

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User
February 11, 2021

+1 for hardware and for trying it on a "known good" hardware as Disco or Nucleo.

JW

ABous.3
ABous.3Author
Associate II
February 11, 2021

Hi all,

Thank you for your advices.

Here is a print screen of micro's state the last time Hard Fault happened:

0693W000007EvjJQAS.pngI will also check hardware with my colleague tomorrow, and keep you in touch.

Best regards

Tesla DeLorean
Guru
February 11, 2021

You want to look at the code disassembly to put the register content in context.

Are the values here volatile, are they flagged in a TIM or SYSTICK interrupt.

Does behaviour change if optimization level dropped?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ABous.3
ABous.3AuthorBest answer
Associate II
February 15, 2021

Hi everyone,

Thank you for your advices.

On friday my colleague saw that some capacitors were missing on my board, and corrected this. My board has been running for the weekend, and no hardfault happened. I am leaving it running a longer time to ensure this was not luck. I also flashed another board with my software and will let it run.

I will keep you informed.

Have a nice week!

Best regards

ABous.3
ABous.3Author
Associate II
February 22, 2021

Hi all,

Just to keep you in touch: I have run my software on two boards for a week, and faced no hardFault. So it seems like the problem was a hardware one.

Thank you for your advices

Best regards