STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7 Hard Fault when RCC at 165 MHz

I have the STM32H7B3I-DK (MCU: STM32H7B3LIH6Q), and I am trying to get the sys_ck close to its maximum frequency of 280 MHz, by running HSI or HSE through PLL. The trouble is that I can only get up to 164 MHz. Any higher and I get a hard fault. Is th...

FSkro.1 by Associate II
  • 1324 Views
  • 1 replies
  • 0 kudos

STM32F767 ZI, Trouble understanding how HAL_I2C_MASTER transmit works. Trying to send 32 bit adc data over I2C

So I am trying to send an ADC value that I receiving on the board over I2C to another device. I have adc_Value as a 32 bit one since the ADC read function on HAL is 32 bits. I want to send this over i2c. Currently I have this.  HAL_ADC_Start(&hadc1);...

HSyed.1 by Associate II
  • 2306 Views
  • 4 replies
  • 0 kudos

Resolved! How to use DMA on complementary timer channels in TIM1

I have been trying to start PWM on TIM1 with complementary channels and use DMA to start the PWM. The problem that I have is that only one of the channels will start when I run the program. DMA channel 2 is being used by TIM1_CH1 and I can't find any...

Mhass.12 by Associate II
  • 4234 Views
  • 4 replies
  • 0 kudos

HAL_Delay stuck when sdram use as data memory

Hi:I have a custom STM32F746NG board with SDRAM IS42S328200D(Address 11 bits 2^11(Row Address)*2^8(Column Address)*32(bit)*4(bank)). My goal is to use sdram as data memory, I followed example in STM32Cube_FW_F7_V1.16.1\Projects\STM32746G-Discovery\Ex...

PWM Timer Slave not getting triggered by Master

Hello, I am trying to set timer 3 as a master to timer 1 without success. Timer3 is outputting the PWM correctly, but timer1 is not getting triggered by Timer3's PWM Signal. What else am I missing?My board is STM32F429 discovery Here are my settings ...

0693W00000Bc447QAB.png 0693W00000Bc442QAB.png 0693W00000Bc44CQAR.png 0693W00000Bc455QAB.png
Xxoyo.1 by Associate III
  • 2241 Views
  • 3 replies
  • 0 kudos