when i use USB High speed to achieve Communication Device Class(VCP USB-to-RS232 bridge to realize a virtual COM port),If not set USBHS Interrupt highest priority Communicate with the computer for a period of time the program enter hardFault。
Thanks for your help.But I do not see the "FMC do not support unaligned acces" in H745 Errata. Another problem is that this only happens on the M7 platform.Does it mean that only M7 has this problem.