User Activity

In the data sheet and reference manual of STM32L073, LCD_VLCD1 is 42pin and LCD_VLCD2 is 37pin, but in STM32CubeMX, the instructions are reversed.Also, at 1/3 bias, the reference manual is supposed to use LCD_VLCD1 and LCD_VLCD2, but STM32CubeMX will...
I am using STM32L073.When using this ADC, the EOC of the flag ADC_ISR for which AD conversion has been completed does not change unless the EOCIE of ADC_IER is set.is it right.
Hi,In STM32L073, the ADC conversion time is stated as 0.875us with 12-bit resolution.Even in the actual test, it has been confirmed by the continuous operation of 1ch of ADC.However, I set the ADC results to be transferred by DMA, the ADC conversion ...
Is it possible to set the LCD drive voltage to 4.5VDC in STM32L073?When using a VA liquid crystal panel an LCD, it is said that it cannot be driven by 3.6VDC.
Kudos from