STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32N6 series DCMI module

I am very new to this field !! So last I had posted regarding the interfacing of DCMI and I got relevent doucuments which where not enough for me to understand the DCMI module. So could you please send relevant videos of interfacing DCMI module step ...

nishanth by Associate II
  • 1033 Views
  • 2 replies
  • 0 kudos

Resolved! STM32C011 invalid temerature read by ADC

I've used CubeIDE 1.18.1 to create a small project based on a STM32C011F6. The ADC is configired thru Cube to read Vref+, temp sensor and another external voltage.Cube has therefore created an init function MX_ADC1_Init which is called at during star...

MWebj by Associate III
  • 599 Views
  • 1 replies
  • 0 kudos

STM32F3 GPIO Bit-banding question

Hello, I have purchased and used the NUCLEO-F303RE board. I am trying to control the LED (PA5) using bit-banding. With reference to the reference manual, I confirmed that the address of GPIOA starts from 0x48000000. Then, I found and read the PM0214 ...

giwonKIM by Associate III
  • 1007 Views
  • 6 replies
  • 4 kudos

Resolved! STM32G070CBTx Multichannel ADC & DMA Config Help!

Hi everyone,I'm working on a multichannel ADC1 + DMA setup using an STM32G070CBTx MCU, and I'm running into an issue with buffer readings.My ADC configuration involves 8 channels mapped as follows:Joystick: ADC1_IN9 (Rank 1) and ADC1_IN10 (Rank 2)Bat...

image.png image.png