cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G031 issue when using CubeProgrammer with UART bootloader

Pinglei
Associate II

STM32G031Y8Y6TR is now burning some problems would like to consult

Serial port 1 after burning OK, when burning again can not read the MCU situation, help to see what will be the reason, how to solve, thanks a lot.

Pinglei_0-1739759751624.png

Pinglei_1-1739759758399.jpegPinglei_2-1739759764689.jpegPinglei_3-1739759769529.jpeg

 

 

5 REPLIES 5
TDK
Super User

Are you holding BOOT0 high during reset so it enters the bootloader?

Is ground connected between board and UART module?

If you feel a post has answered your question, please click "Accept as Solution".

There is ground between the board and the UART module, and the BOOT0 remains at a high level of 5V

Pinglei
Associate II

Please look again ,thanks a lot.

5V ??

Perhaps instead of kicking the thread you make your presentation of the issue more clear and compelling?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
EniRot99
Associate III