STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103C8T6 with MSL 2 and 3? Please advise.

We bought STM32F103C8T6, COO is Malaysia, but MSL on the label is MSL 2, is it correct ? Because we found official datasheet for this P/N is MSL 3. Could you please help explain why one p/n with two MSL ? Thank you.

ENeoh.1 by Associate II
  • 2133 Views
  • 2 replies
  • 0 kudos

external QSPI flash issue

we are using stm32h745 chip,we want to 64 mb algorthim but in dfp file has 128 mb algorthim only,Controller how to accesess through 64 mb qspi flash.

Nredd.1 by Associate III
  • 1780 Views
  • 6 replies
  • 1 kudos

Odd and Even CAN bus ID's FilterConfig

Hi, I am working with STM32F103 and configured CAN filter to receive ODD and EVEN ID's to FIFO0 and FIFO1 accordingly: CAN_FilterTypeDef sFilterConfig; sFilterConfig.SlaveStartFilterBank = 28; sFilterConfig.FilterActivation = ENABLE; sFilterCo...

JBond.1 by Senior
  • 890 Views
  • 1 replies
  • 0 kudos

Application cross two Bank, possible?

For stm32h7b3 , there are two Bank of flash, and each 1M, We are designing a big application which code size may exceed 1m.So may I know if possible to ​use two bank for this application? Any limitations for it?Or if possible to put application to ex...

jiangpen by Associate II
  • 1487 Views
  • 3 replies
  • 0 kudos

Resolved! FMC interfacing lcd screen minor issue

I have nearly managed to interface one lcd screen(ili9341 16bit parallel fmc intel 8080 protocol) with my stm32 device but I am stuck at the very last step.I have connected the screen wires to the mcu , I have configured fmc from cube mx correctly , ...

SMour.1 by Associate III
  • 3069 Views
  • 4 replies
  • 0 kudos

Unable to Communicate STM32G4 Nucleo-32 with SPS30 in I2C Mode!

Having difficulty to communicate with SPS30 on I2C. As a beginner I am having difficulty to understand how to debug the problem as it just returns 255 in in_buff. This topic may sound to broad, however, If someone can guide me the direction to make ...

PJ.3 by Associate
  • 1357 Views
  • 1 replies
  • 0 kudos