STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I am using STM32H7 board and integrated an SD card using SPI and able to mount it in "/". I am storing a file inside the SD card.

HAL_Delay (500); fresult = f_mount(&fs, "/", 1);  if (fresult != FR_OK)   Serial_PutString ("ERROR!!! in mounting SD CARD...\n\n");  else  {   Serial_PutString("\n\r SD CARD mounted successfully...\n\n");  fresult = f_open (&fil, "zephyr_20210506_nbi...

JJoy.1 by Associate III
  • 3894 Views
  • 5 replies
  • 0 kudos

Resolved! Problems with reading through SPI with DMA on STM32F407

Hi!So I configured my SPI to work with DMA and with external CS. Before my main loop I set CS high, and everytime before I initialize communication on SPI with DMA i set CS low. Then, after communication is done I go to interrupt on that event and se...

0693W00000D148wQAB.png 0693W00000D149pQAB.png
bmak by Senior
  • 5516 Views
  • 5 replies
  • 0 kudos

using stm32f051 disco+ lcd2004 I2C connection, Between 30min~3 hours after booting, lcd has no indication on the screen or letters, but the indication does not change (count No) Which part is good to look at? Is there any particular problem with lcd?

#include "i2c-lcd.h"   extern I2C_HandleTypeDef hi2c1; // change your handler here accordingly     #define SLAVE_ADDRESS_LCD 0x4E // change this according to ur setup       long ErrCnt_ERR=0;   long ErrCnt_Tout=0;   long ErrCnt_Busy=0;   HAL_St...

Kse.1 by Associate II
  • 934 Views
  • 0 replies
  • 0 kudos

PROBLEM IN "STM32h743" "DMA" "UART" in "IAP" MODE

HELLO EVERYONEI run my micro in IAP Mode then load other program to him with uart1 . in this program I start UART with DMA and toggle one Pin . when the circuit start working , everything work well and pin is toggle but the UART DMA send out zero. V...

mika.1 by Associate II
  • 1986 Views
  • 8 replies
  • 0 kudos

I2C CMSIS STM32F303RE

Hello again. I'm having this problem with I2C with the STM32F303RE.I have this array of data I want to send via I2C to a sensor.std::uint8_t conf_bytes[2] = {0xF4, 0x03}; periph::I2C::write_data(I2C1, BME_ADDR, 2U, conf_bytes); BME_ADDR is the addr...

0693W00000D1A7VQAV.png 0693W00000D1A7pQAF.png

SystemClock Settings for STM32L0 mcu

HiI have my own board, with STM32L053C8T6TR. And I set clock and program failed here: while (LL_RCC_HSE_IsReady ()! = 1) {};void SystemClock_Config(void) {   LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_PWR); // clock pro PWR controller LL_PW...

0693W00000D1DhCQAV.png

STM32F407VET6 recognized as Mass Storage Device

Hello, guys. Bought and STM32 board, tried to upload .hex file on it from ST-Link Utility, but when tried to connect board, received "No ST-LINK detected!". Checked in Device Manager - board appear as Mass Storage device(No ST-Link Debug, just storag...

YSukh.1 by Associate
  • 657 Views
  • 0 replies
  • 0 kudos

STM32L562, dynamically modify serial port configuration.

Excuse me, how to gracefully and effectively change the TX pin "inversion" of usart3 during the operation of MCU program?In addition, can I ask questions in Chinese? Every question needs the cooperation of translation software. I'm afraid there will ...

MShao.1 by Associate III
  • 1575 Views
  • 2 replies
  • 0 kudos