User Activity

Hello,I'm struggeling a bit in understanding the whole features of possible RTC improvements. General information, right now I'm using a STM32L051 and a external 32,768kHz Oscillator for the RTC. It's working in general, but the OSC has +/-30ppm whic...
Hello,I've tested a few weeks now without solution, hopefully somebody can help me with this topic.I try to reach the Low Power mode (LP Run or LP Sleep), but when I enter it, the consumption is still at 150µA (~270µA in debug mode). I even tested wi...
Hello,I have problems installing the Cube Programmer. During installation it fails to execute some batch files (first one "populateApi.bat"). If I continue installation anyway, the installed Cube Programmer can't be opened and can't be uninstalled, o...