STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

The Support Level of STM32MAT-TARGET for STM32H7xx series

Hi everyone,I'm facing a problem where I don't have the flexibility to configure every peripheral of STM32H742VIT6 from Simulink. For instance when I want to use a TIM block in Simulink, it does not allow me to do so. Furthermore, the support for FDC...

ÇSütu.1 by Associate II
  • 1608 Views
  • 2 replies
  • 0 kudos

Type of Battery for STM32U585 MCU

Hi All,We are planning to use STM32U585 series MCU. while going through the datasheet it is mentioned as Vbat with internal charging circuit. Whether we use non rechargeable battery or Supercapacitor for Vbat pin? or it can be used only rechargeable...

SSiva.11 by Associate
  • 2068 Views
  • 3 replies
  • 0 kudos

Is there a way to output Vref+/2 in an STM32L4R5ZI?

Hi!I'm using the STM32L4R5ZI's DAC to generate a signal, after that I'm using a differential amplifier to eliminate the DC level of the signal (since DAC can only output from 0 to Vref+). For that ampifier I need the value in witch the signal is cent...

DMart.16 by Associate II
  • 1534 Views
  • 2 replies
  • 0 kudos

STM32H743 DMA not working

In the program that transmits the value received from uart4 to uart5, I want to move the value received from uart5 to another buffer, but I move it to HardFault_Handler.what is the reason?And please check if the method of receiving data using the dma...

BPark.5 by Associate II
  • 2880 Views
  • 5 replies
  • 0 kudos

Problem Implementing QUADSPI

I have few confusions:How do you activate QUADSPI Indirect mode ? Does MX_QUADSPI_Init() activates the Indirect mode ? Is the default mode Indirect mode after initialising QUADSPI ? Do you need to activate it somehow from the software or some command...

SLuit.1 by Associate III
  • 666 Views
  • 0 replies
  • 0 kudos

I am using STM32L471 controller, I just want to ask that what is the maximum value of decoupling capacitor which can be used at JTAG SWDIO pin of controller, so that there would not be any issue during programing of controller using SWD 4MHz setting.

I am using STM32L471 controller, I just want to ask that what is the maximum value of decoupling capacitor which can be used at JTAG SWDIO pin of controller, so that there would not be any issue during programing of controller using SWD 4MHz setting.

AC1 by Associate
  • 1735 Views
  • 3 replies
  • 0 kudos