Skip to main content
MBeal.1
Associate
May 3, 2021
Solved

Flash Loader Demonstrator cannot open port

  • May 3, 2021
  • 3 replies
  • 4147 views

I have a Win10 notebook computer. When I run the Flash Loader Demonstrator, it correctly finds the com port being used (the only one) but when I click 'Next' it always says ​"Cannot open the com port, the port may be used by another application". This is from a clean boot, and even on other computers. How do I fix this?

This topic has been closed for replies.
Best answer by Tesla DeLorean

The Demostrator app is deprecated, try using the STM32 Cube Programmer in UART mode

3 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
May 3, 2021

The Demostrator app is deprecated, try using the STM32 Cube Programmer in UART mode

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MBeal.1
MBeal.1Author
Associate
May 4, 2021

​Thank you!

Unfortunately, I still get the same error message:

"Cannot open port COM3, it may be used by another application or the port name is invalid."

?

Tesla DeLorean
Guru
May 4, 2021

What's the COM port associated with? An FTDI or SiLabs adapter?

Can you open the port in RealTerm or some other terminal app?

Is it associating it with some other driver, Microsoft Serial Mouse, or Location API, or such?

Check Tasks and Services that could be running.

Failing that you're likely going to need to get your IT staff to determine what is attaching.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..