STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FMC/FSMC ECC computation

Hello, guys!I have a quick question about FSMC's ECC routine.From what I understood, the workflow goes like this:1) Enable ECC computationSET_BIT(hnand->Instance->PCR, FMC_PCR_ECCEN);2) Write data to the target device3) Get the computed ECCwhile (__F...

PMera.1 by Associate III
  • 1764 Views
  • 2 replies
  • 0 kudos

STM32F7 SMBUS vs STM32F4 SMBUS

Differences in setting up for SMBUS:On F4, I set the following bits in CR1: PEC POS ENPEC SMBTYPE SMBUSOn F7, are there similar bits?I see PECEN - is that the same as ENPEC on F4?How do you set up SMBUS on F7? (on F4, it was done with SMBTYPE and SMB...

TAnde.5 by Associate II
  • 851 Views
  • 0 replies
  • 0 kudos

Resolved! ADC noise on stm32f401

I've been messing around with a LMT86 temperature sensorThis sensor is deemed high output impedance as the documented loads it drives is 50uA.ADC noise on STM32 isn't 'new'. Just that for a first time I'm observing such volatility up close. The probl...

0693W00000Dnmj4QAB.png 0693W00000DnmjsQAB.png 0693W00000DnmlPQAR.png 0693W00000DnmmwQAB.png
andrewg by Associate III
  • 10601 Views
  • 16 replies
  • 0 kudos

stm32f429 shortage

Hello everyone ; I dont know if this is the right place to write ; we are using stm32f429 in our products we use about 20K / year . we are doing the plan for the next year we are getting a long ..very long shippng dates like 80 weeks ! even now we...

Trouble with SDCARD - SDMMC_FLAG_RXOVERR

I'm attempting to connect an adafruit SD card reader via SDIO to a Nucleo L476RG.I'm reading through the source code to do a test of the basic read/write functions.Initialization and getting card info is successful. if (HAL_SD_Init(&hsd1)!=HAL_OK){...

STM32L071x8 GPIO configuration as analog input or input

Hello,what is the difference between configuring GPIO pins from software and leave as default(no code). does it have an impact on other register settings that are not being set/clear in default configuration. because I am having a problem when I leav...

DRamo.1 by Associate II
  • 2180 Views
  • 5 replies
  • 0 kudos

Resolved! There seem to be a mismatch in the STM32H747 documentation: The 176 pin version should have an VDDDSI pin, but it's missing in the pin definition and in the pinout. Is it a typo?

According to the STM32H747xI/G datasheet, the STM32H747IG has a VCAPDSI pin, but no VDDDSI pin at all.I'm sure i get something wrong here, because without VDDDSI pin, the VCAPDSI pin would be a miraculous source of energy! ;)But seriously: do i have ...

AHoll.2 by Associate II
  • 2752 Views
  • 4 replies
  • 2 kudos